Skip to main content
Adrian Chmiel
Associate
Apr 1, 2026 10:31 PM UTC
Solved

STM32WB5MMG - cannot change device name/model

Hi,

I'm working on a project with your STM32WB5MM module, I managed to enable ZigBee and connect to the network, but I'm having trouble changing the device name, it keeps identifying itself as default value (STM32WB).

ZigBee Stack: 1.24.0
FW Type : FFD Zigbee stack

In function APP_ZIGBEE_StackLayersInit() I add:

struct ZbZclBasicServerDefaults basic_defaults = {
 .app_version = 1, 
 .stack_version = 2, 
 .hw_version = 1, 
 .mfr_name = "0TestName", 
 .model_name = "0LOCKZ1A", 
 .date_code = "02026-03-31", 
 .power_source = ZCL_BASIC_POWER_DC, 	
 .sw_build_id = "0v1.0" 
};

static void APP_ZIGBEE_StackLayersInit(void)
{
 APP_DBG("APP_ZIGBEE_StackLayersInit");

 zigbee_app_info.zb = ZbInit(0U, NULL, NULL);
 assert(zigbee_app_info.zb != NULL);

// uint8_t device_name[] = {"0TestDevice"};
// device_name[0] = 10;
// ZbZclBasicWriteDirect(zigbee_app_info.zb, ZB_ENDPOINT_BCAST, ZCL_BASIC_ATTR_MFR_NAME, device_name, device_name[0]);

 basic_defaults.mfr_name[0] = strlen((char*)basic_defaults.mfr_name)-1;
 basic_defaults.model_name[0] = strlen((char*)basic_defaults.model_name)-1;
 basic_defaults.date_code[0] = strlen((char*)basic_defaults.date_code)-1;
 basic_defaults.sw_build_id[0] = strlen((char*)basic_defaults.sw_build_id)-1;
 ZbZclBasicServerConfigDefaults(zigbee_app_info.zb, &basic_defaults);

 /* Create the endpoint and cluster(s) */
 APP_ZIGBEE_ConfigEndpoints();

 /* USER CODE BEGIN APP_ZIGBEE_StackLayersInit */

 /* USER CODE END APP_ZIGBEE_StackLayersInit */

 /* Configure the joining parameters */
 zigbee_app_info.join_status = (enum ZbStatusCodeT) 0x01; /* init to error status */
 zigbee_app_info.join_delay = HAL_GetTick(); /* now */
 zigbee_app_info.startupControl = ZbStartTypeJoin;

 /* Initialization Complete */
 zigbee_app_info.has_init = true;

 /* run the task */
 UTIL_SEQ_SetTask(1U << CFG_TASK_ZIGBEE_NETWORK_FORM, CFG_SCH_PRIO_0);
}

But it's still identifying itself with default values. What could I be doing wrong?
Is there a way to read the parameters I'm saving to check their validity?
I also tried direct recording using ZbZclBasicWriteDirect() but also no reaction.

Best regards,
Adrian Chmiel

OuadiBest answer
ST Technical Moderator
Apr 13, 2026 2:58 PM UTC

Hello @Adrian Chmiel,

Thanks for contacting us on the ST Community.

Please find the answer below:

To configure the default ZCL Basic Server attributes, you need to meet the ZCL data format used by ZbZclBasicServerDefaults — in particular, string attributes are encoded as length-prefixed strings rather than standard null-terminated C strings.

As an example, you can refer to the following project available on the official Git: 

STM32CubeWBA/Projects/NUCLEO-WBA55CG/Applications/Zigbee/Zigbee_OnOff_Client_SED/STM32_WPAN/App/app_zigbee.c at main · STMicroelectronics/STM32CubeWBA · GitHub

Regards,

Ouadi

1 reply

OuadiBest answer
ST Technical Moderator
Apr 13, 2026 2:58 PM UTC

Hello @Adrian Chmiel,

Thanks for contacting us on the ST Community.

Please find the answer below:

To configure the default ZCL Basic Server attributes, you need to meet the ZCL data format used by ZbZclBasicServerDefaults — in particular, string attributes are encoded as length-prefixed strings rather than standard null-terminated C strings.

As an example, you can refer to the following project available on the official Git: 

STM32CubeWBA/Projects/NUCLEO-WBA55CG/Applications/Zigbee/Zigbee_OnOff_Client_SED/STM32_WPAN/App/app_zigbee.c at main · STMicroelectronics/STM32CubeWBA · GitHub

Regards,

Ouadi