Question
STM32WB5MM OTA Application at a different address
I have multiple questions:
1. Is there a limit on the firmware size in STM32WB series? If yes, what is the limit?
2. Is there a limit on the firmware size of the OTA application in STM32WB series? If yes, what is the limit?
3. I want to perform OTA at a different address, not 0x08007000. Is it possible?