Skip to main content
Associate
Aug 5, 2024 6:09 AM UTC
Question

STM32WB55RGV6 No St-Link Detected

I've been struggling to connect my nucleo board via ST-Link, I've tried uninstalling everything, reinstalling and my computer still won't detect the board when I plug it in. It's always just COM-3 device or whatever port I use. Tried installing the STSW-LINK009 driver directly from the STM website but still nothing.

This topic has been closed for replies.

9 replies

STTwo-32
ST Technical Moderator
Aug 5, 2024 7:29 AM UTC

Hello @jvu and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Could you please try to connect your MCU to the STM32CubeProgrammer. Don't forget to check that all pins are correctly wired (if it is a Nucleo, ensure that the JP1 is fitted on the USB_STL and that you are connecting the USB cable throw the CN15).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
jvuAuthor
Associate
Aug 6, 2024 3:51 AM UTC

Thank you for the reply!

I've downloaded the programmer and can connect via J-Link. Is there anything I can do or change to be able to connect to the NUCLEO board with ST-LINK? 

STTwo-32
ST Technical Moderator
Aug 6, 2024 4:39 AM UTC

Could you share a picture of you're connections (board to PC and ST-link if it is not an eval board). Also, a screenshot of the error that you are receiving will trying to connect to CubeProgrammer with ST-LINK  will be really helpful.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.