Skip to main content
Associate
Sep 21, 2025 6:56 PM UTC
Question

[STM32WB55 + Zigbee_onoff_client_sed] “Target is not responding”

I’m developing a Zigbee end-device app on STM32WB55 (Zigbee_OnOff_Client_SED), following ST’s Zigbee guide, but my debugger keeps showing “Target is not responding, retrying…” . I disabled low power (CFG_FULL_LOW_POWER=0 / CFG_LPM_SUPPORTED=0), set Connect under reset in CubeIDE, and updated the ST-LINK, but the issue persists and the node won’t join my network. Could this be the CPU2 wireless firmware (RFD vs FFD) or a FUS/Option Bytes problem? If anyone has a proven recovery checklist (mass erase under reset, correct CPU2 image, OB settings, etc.) or other tips to make SWD reliable and get the device to join, I’d really appreciate it.

This topic has been closed for replies.

2 replies

Ghofrane GSOURI
ST Technical Moderator
Sep 23, 2025 10:15 AM UTC

Hello @Azizzr02 

I believe posting this question in the ST Wireless Forum could help you get more targeted advice, especially regarding whether your  issue is related to the CPU2 wireless firmware (RFD vs FFD), the FUS version, or Option Bytes configuration.

 

BR,

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
Oct 13, 2025 9:58 AM UTC

Hi @Azizzr02,

The debugger is disabled by default for all Zigbee Sleepy applications in order to achieve a best low power consumption.

For debugging purpose, you have to set these two flags in app_conf.h as follow :


- #define CFG_FULL_LOW_POWER             0

- #define CFG_DEBUGGER_SUPPORTED   1

Best regards,

Ouadi