Question
STM32WB55 write OTP fails
I have a board NUCLEO-WB55RG and STM32CubeProgrammer v2.12.0, I'm trying to write OTP area to address 0x1FFF7000, but I got errors.
I edit with GUI and I got error message: "Memory edition verification failed", with CLI I have this error:
./STM32_Programmer_CLI -c port=swd -w32 0x1FFF7000 0xAAAAAAAA
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
ST-LINK SN : 066BFF5XXXXXXXXXXXXXX
ST-LINK FW : V2J40M27
Board : NUCLEO-WB55RG
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev X
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled
Write 32-bit data
w @0x1fff7000: 0xaaaaaaaa
Downloading...
[==================================================] 100%
Error: Failed to download data! If it's a Flash memory, it may be not erased or protectedI also tried to update firmware of st-link but I got always the same errors.