Question
STM32WB55 Running BLE Stack not resettable using hardware reset
I have a custom board running the BLE (full) stack. The application code is written using the Zephyr RTOS. The power source is a CR2032 coin cell battery. After operating for a while (the actual times vary), some units (not all as far as I know) get into a state where I cannot get the device back by asserting the reset signal on the processor. Only a POR will recover the device.
Some notes:
- I've measured the current consumption in this state and it is a consistent 400-500uA. The current consumption increases when I assert reset so I know the reset signal is getting asserted
- It does not seem to be going into the bootloader as it doesn't come up as a DFU device over USB.
- The ST-LINK debugger cannot connect to the target using any mode (Hot-plug, normal, or under reset).
How can the chip get into such a state where power cycling is necessary to effectively restart it? Has anyone seen something like this before?