Skip to main content
SteveJ
Associate II
May 18, 2025 11:01 AM UTC
Solved

STM32WB55 radio comms without bluetooth?

Hi,

I have to use the transceiver for pure RF communications and implement my own protocole.
After checking several boards, I've be recommended the P-NUCLEO-WB55 but from all the doc and example I find, the transceiver is used for BlueTooth communications, which I don't need at all.
Is it possible to use its transceiver RF without BLE, Zigbee, etc... as a simple 2.4Ghz range transmitter and receiver?

If not, which MCU should I get, that includes a dev board offering AD, DA and pure RF ?
Thanks for any light.

 

Steve

This topic has been closed for replies.
FilipKremen
FilipKremenBest answer
ST Employee
May 19, 2025 8:41 AM UTC

Hello,

you can create your own protocol built on 802.15.4.

Please have a look here for more information.

Connectivity:Introduction to 802 15 4 - stm32mcu

 

Best regards,

ST support

4 replies

FilipKremen
FilipKremenBest answer
ST Employee
May 19, 2025 8:41 AM UTC

Hello,

you can create your own protocol built on 802.15.4.

Please have a look here for more information.

Connectivity:Introduction to 802 15 4 - stm32mcu

 

Best regards,

ST support

Andrew Neil
Super User
May 19, 2025 9:13 AM UTC

@SteveJ wrote:

If not, which MCU should I get, that includes a dev board offering AD, DA and pure RF ?


Does the RF need to be 2.4GHz ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
SteveJ
SteveJAuthor
Associate II
May 19, 2025 9:49 AM UTC

Andrew,

Yes it has to be in the 2.4GHz range, not sub GHz.

Steve

Steve JORDI - M.Sc. in Geophysics - Volcanology - Scientific Advice - Software Development
STTwo-32
ST Technical Moderator
May 19, 2025 9:51 AM UTC

Hello @SteveJ 

As suggested by @FilipKremen, the 802.15.4 is a widely used communication protocol that enables the creation of Wireless Personal Area Networks (WPAN). So, it will be a good idea to use it.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.