Question
STM32WB55 power consumption
Hi,
I have a board which has a STM32WB55RGV6 MCU and i have a problem. When i connected my board to Power supply, it consumes just 13 mA. But then suddenly, it increased 94 mA. I measured resistance between GND and VDD_MCU pins. I was 53 ohm. I understand that the problem is in there. But i dont understand everythings are working properly. I use SPI1, I2C, SPI2, Analog pins, USB, GPIO pins. There is no problem about them.
Even if it is in sleep, it consume 82 mA. There is a problem but where is it. How can i solve it?
Thanks for your interest