Solved
[STM32WB55 Nucleo] SHCI_FUS_CMD_NOT_SUPPORTED Error on SHCI_C2_FLASH_EraseActivity
I updated The FUS of my STM32WB55 Nucleo Board to FUS v2.2.0.0 and the BLE Stack to v1.24.0.3
After this change Flash erase operations fail at the call of `SHCI_C2_FLASH_EraseActivity` with the error code `SHCI_FUS_CMD_NOT_SUPPORTED`
Additionally BLE does not advertise anymore.
The log from the `Read FUS infos` returns some warnings:
notably:
10:35:12 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
10:35:12 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
10:35:12 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
10:35:12 : Warning: Option Bytes are unchanged, Data won't be downloadedThe entire log:
10:35:12 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
10:35:12 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
10:35:12 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
10:35:12 : Warning: Option Bytes are unchanged, Data won't be downloaded
10:35:12 : Time elapsed during option Bytes configuration: 00:00:00.000
10:35:12 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
10:35:12 : Opening and parsing file: 0x495_FUS_Operator.bin
10:35:12 : Memory Programming ...
10:35:12 : File : 0x495_FUS_Operator.bin
10:35:12 : Size : 8.00 KB
10:35:12 : Address : 0x08000000
10:35:12 : Erasing memory corresponding to segment 0:
10:35:12 : Erasing internal memory sectors [0 1]
10:35:12 : Download in Progress:
10:35:12 : File download complete
10:35:12 : Time elapsed during download operation: 00:00:00.276
10:35:12 : Application is running, Please Hold on...
10:35:12 : Reconnecting...
10:35:12 : Reconnected !
10:35:13 : FUS_STATE_IDLE
10:35:13 : Read FUS state command execution finished
10:35:13 : UPLOADING ...
10:35:13 : Size : 4 Bytes
10:35:13 : Address : 0x20010010
10:35:13 : Read progress:
10:35:13 : Data read successfully
10:35:13 : Time elapsed during the read operation is: 00:00:00.000
10:35:13 : UPLOADING ...
10:35:13 : Size : 4 Bytes
10:35:13 : Address : 0x20010014
10:35:13 : Read progress:
10:35:13 : Data read successfully
10:35:13 : Time elapsed during the read operation is: 00:00:00.000
10:35:13 : UPLOADING ...
10:35:13 : Size : 4 Bytes
10:35:13 : Address : 0x8001FFC
10:35:13 : Read progress:
10:35:13 : Data read successfully
10:35:13 : Time elapsed during the read operation is: 00:00:00.000
10:35:13 : UPLOADING ...
10:35:13 : Size : 4 Bytes
10:35:13 : Address : 0x58004080
10:35:13 : Read progress:
10:35:13 : Data read successfully
10:35:13 : Time elapsed during the read operation is: 00:00:00.000
The option bytes:
{
"deviceId" : 1173,
"bitNameToValue" : {
"RDP" : 170,
"BOR_LEV" : 0,
"nBOOT0" : 1,
"nBOOT1" : 1,
"nSWBOOT0" : 0,
"SRAM2RST" : 0,
"SRAM2PE" : 1,
"nRST_STOP" : 1,
"nRST_STDBY" : 1,
"nRSTSHDW" : 1,
"WWDGSW" : 1,
"IWDGSTDBY" : 1,
"IWDGSTOP" : 1,
"IWDGSW" : 1,
"IPCCDBA" : 0,
"ESE" : 1,
"PCROP1A_STRT" : 511,
"PCROP1A_END" : 0,
"PCROP_RDP" : 1,
"PCROP1B_STRT" : 511,
"PCROP1B_END" : 0,
"WRP1A_STRT" : 255,
"WRP1A_END" : 0,
"WRP1B_STRT" : 255,
"WRP1B_END" : 0,
"SFSA" : 208,
"FSD" : 0,
"DDS" : 1,
"C2OPT" : 1,
"NBRSD" : 0,
"SNBRSA" : 16,
"BRSD" : 1,
"SBRSA" : 0,
"SBRV" : 249856
}
}
How can I solve this issue?