Skip to main content
LHege.1
Associate III
Dec 15, 2022 12:43 PM UTC
Question

STM32WB55: Maximal execution time running the code on QUADSPI

Hi there

How to calculate the maximal possible CPU execution time for the STM32WB55 when running fetching the code from external flash?

Kind Regrads

This topic has been closed for replies.

3 replies

ChahinezC
Associate II
Dec 15, 2022 4:06 PM UTC

Hello @Community member​,

The CPU can execute code from the Quad-SPI memory when using the memory-mapped mode. I advise you to refer to the table 2 of the AN4760 where you can find the maximum QUADSPI speed of STM32WB55, of course added to the datasheet of the product.

Regards,

Chahinez.

Tesla DeLorean
Guru
Dec 15, 2022 7:02 PM UTC

Dependent on multiple factors.

Not an inherently cached architecture.

Suggest you benchmark with DWT's CYCCNT to evaluate with your own HW, and code construction.

Figure each instruction is 16-bit wide, and you know the QSPI clocking speed, and CS cycles, you can probably put a floor in the execution speed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LHege.1
LHege.1Author
Associate III
Dec 16, 2022 9:29 AM UTC

Hi all,

Thanks for the quick answers. I did a calculation with this Information for a best case scenario:

  • Quadspi: 4 Lane mode
  • DDR mode enabled
  • SIOO mode enabled (Continuous-read mode)
  • Maximum Quadspi clock speed is 50 MHz (AN4760)
  • 16-bit instruction length (for 32-bit RISC architecture)

So if we execute a code that contains no jumps, the code can be fetched without sending the address again. 

  • Per clock we get 2 bit (DDR) per line so 8 bit per clock
  • We need 2 clocks to fetch one 16 bit instruction
  • So the maximal execution speed would be 25 MHz

Can someone verify this numer for a best case scenario? Are there any necessary wait cycles that I missed?