Skip to main content
Jsilv.1
Associate II
May 8, 2020 12:57 PM UTC
Question

STM32WB55 Low Power Mode wakeup using BLE stack

Hi,

I can enter STOP Mode 2 while not using the ST Sequence (UTIL_SEQ). I disable interruptions, clear the pending ones and just let the RTC to wake me up.

HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xFFFF, RTC_WAKEUPCLOCK_RTCCLK_DIV8);
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);
UTIL_LPM_EnterLowPower( );
HAL_ResumeTick();
SYSCLKConfig_STOP(); //restore clocks and so on...

But when I do the same in void UTIL_SEQ_Idle( void ) I get wake up inmediatly...

I tried to disable every single interrupt (I'm using GPIOS interrupts, RTC, Alarms, UART, Timer2 and the BLE stack for P2P_Server). Who is waking me up from sleep?

void UTIL_SEQ_Idle( void )
{
 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
 UTIL_LPM_SetStopMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE);
 UTIL_LPM_SetStopMode(1U << CFG_LPM_APP_BLE, UTIL_LPM_ENABLE);
 EXTI->PR1 = 0xFFFFFFFF;
 EXTI->PR2 = 0xFFFFFFFF;
 RTC_WAKEUPCLOCK_CK_SPRE_16BITS);
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 HAL_SuspendTick();
 HAL_NVIC_DisableIRQ(WWDG_IRQn);
 HAL_NVIC_DisableIRQ(EXTI0_IRQn);
 HAL_NVIC_DisableIRQ(EXTI1_IRQn);
 HAL_NVIC_DisableIRQ(EXTI2_IRQn);
 HAL_NVIC_DisableIRQ(DMA1_Channel1_IRQn);
 HAL_NVIC_DisableIRQ(DMA1_Channel2_IRQn);
 HAL_NVIC_DisableIRQ(TIM2_IRQn);
 HAL_NVIC_DisableIRQ(EXTI15_10_IRQn);
 HAL_NVIC_DisableIRQ(RTC_Alarm_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_DisableIRQ(HSEM_IRQn);
 HAL_NVIC_DisableIRQ(USART1_IRQn);
 HAL_NVIC_DisableIRQ(TIM1_UP_TIM16_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_DisableIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_ClearPendingIRQ(WWDG_IRQn);
 HAL_NVIC_ClearPendingIRQ(RTC_WKUP_IRQn);
 HAL_NVIC_ClearPendingIRQ(EXTI0_IRQn);
 HAL_NVIC_ClearPendingIRQ(EXTI1_IRQn);
 HAL_NVIC_ClearPendingIRQ(EXTI2_IRQn);
 HAL_NVIC_ClearPendingIRQ(DMA1_Channel1_IRQn);
 HAL_NVIC_ClearPendingIRQ(DMA1_Channel2_IRQn);
 HAL_NVIC_ClearPendingIRQ(TIM2_IRQn);
 HAL_NVIC_ClearPendingIRQ(EXTI15_10_IRQn);
 HAL_NVIC_ClearPendingIRQ(RTC_Alarm_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_ClearPendingIRQ(HSEM_IRQn);
 HAL_NVIC_ClearPendingIRQ(USART1_IRQn);
 HAL_NVIC_ClearPendingIRQ(TIM1_UP_TIM16_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_TX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_RX_IRQn);
 HAL_NVIC_ClearPendingIRQ(IPCC_C1_TX_IRQn);
 
 HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xFFFF, RTC_WAKEUPCLOCK_RTCCLK_DIV8);
 HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);
 UTIL_LPM_EnterLowPower( );
 HAL_ResumeTick();
 SYSCLKConfig_STOP();
}

This topic has been closed for replies.

3 replies

Jsilv.1
Jsilv.1Author
Associate II
May 18, 2020 10:31 AM UTC

Please, any input on this?

Jsilv.1
Jsilv.1Author
Associate II
May 20, 2020 8:02 AM UTC

Tried to stop advertising BLE using

aci_gap_set_non_discoverable();

But I wake up in the same way.

Jsilv.1
Jsilv.1Author
Associate II
May 21, 2020 7:12 AM UTC

Surprisingly the file Src/stm32_lpm_if.c was empty, function signatures were generated but anything inside the function body.

It might be a CubeMX bug when generating a Makefile project.

Last question, it is possible to left BLE discoverable while the other CPU is in STOP MODE 2?