Skip to main content
Associate II
Jul 1, 2024 3:01 PM UTC
Solved

STM32WB55 GPIO toggle in cortex M0+ Core is Possible

Hi everyone,

We recently purchased a NUCLEO-WB55RG Dual Core EVK for R&D purposes. We later realized that in the STM32WB55CGU6TR MCU, the Cortex M0+ core is dedicated to BLE. Is there any possibility of toggling GPIO on the Cortex M0+ core? If so, can anyone share a sample code for this?

Thanks in advance!

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 1, 2024 3:29 PM UTC

Hello @pippalla_chakravarthi 

CM0+ is a closed system really dedicated to Wireless Stack. So, you can't use it for other purpose.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Tesla DeLorean
Guru
Jul 1, 2024 3:25 PM UTC

Too what end?

The TIM peripherals can toggle pins associated with them, with no user intervention.

You should be able to do TIM+DMA+GPIO to output a pattern file to pin(s) on a single GPIOx bank

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 1, 2024 3:29 PM UTC

Hello @pippalla_chakravarthi 

CM0+ is a closed system really dedicated to Wireless Stack. So, you can't use it for other purpose.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Jul 1, 2024 4:15 PM UTC

Thanks for the reply, @STTwo-32 

I'm working on generating two different trigger signals: one at 60Hz and another at 600Hz, using three PWM signals on three GPIO or timer channels. I attempted to use slave trigger mode for synchronization, but I'm encountering a phase shift in the PWM signals after two or three pulses.

Can you please guide me on the best possible way to achieve this task?

Andrew Neil
Super User
Jul 1, 2024 4:28 PM UTC

That sounds like a new question.

Best to mark the solution here, and then start a new thread for the new question.

Post a reply here with a link to the new thread.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.