Skip to main content
Visitor II
Oct 23, 2026 11:53 PM UTC
Question

STM32WB55: FUS_GET_STATE returns IDLE over SWD but ERROR over USB DFU; all real operations fail with FUS_STATE_ERR_UNKNOWN either way

Board: WeAct STM32WB55 Core Board (STM32WB55CGU6, 1MB flash)
STM32CubeProgrammer: v2.23.0
Connections tested: ST-LINK/V2 clone (SWD, mode=HOTPLUG) and native
                     USB DFU bootloader (port=usb1, H3/BOOT0 held
                     high to 3.3V)

SUMMARY

A wireless-stack upgrade (v1.20.0.2 -> v1.24.0 stack, which also
required a FUS upgrade from v1.1.1 to a newer FUS) was interrupted
partway through due to the target losing USB connection during the
reconnect phase. Since then, the FUS no longer completes any real
operation (fwdelete, fwupgrade all fail with FUS_STATE_ERR_UNKNOWN)
on either interface. FUS_GET_STATE itself gives a confirmed,
repeatable, interface-dependent result -- see point 10 -- which
doesn't correspond to operations actually working on either side.

STARTING STATE (before anything went wrong)

Read via USB bootloader, Read FUS infos:
  FUS State   : FUS_IDLE
  FUS Status  : FUS_NO_ERROR
  FUS Version : v1.1.1.0
  STACK Version: v1.20.0.2
  STACK Address: 0x80CE000

WHAT WAS ATTEMPTED

1. A FUS upgrade was started (v1.1.1 -> v1.2.0, stm32wb5x_FUS_fw_1_2_0.bin
   at 0x080EC000, Verify download ticked, automatic address
   determination OFF, over USB bootloader port=usb1). Starting state
   confirmed via Read FUS infos immediately before: FUS_IDLE /
   FUS_NO_ERROR, FUS v1.1.1.0, STACK v1.20.0.2 at 0x80CE000.

   The log shows the tool proceeding into the old-stack delete step,
   which triggers an internal reset, and the target never returned
   from it:

     FUS state is FUS_IDLE
     FUS status is FUS_NO_ERROR
     Reconnecting...
     Old Firmware delete ...
     Deleting firmware ...
     Reconnecting...
     [stuck here indefinitely, 0% progress]

   The new v1.2.0 FUS image was never opened/written at this point --
   the failure is specifically in the delete-old-stack step, before
   any new image transfer begins. BOOT0 was not held through this
   internal reset (held momentarily via button rather than a
   continuous jumper), which is suspected as the proximate cause of
   the target not coming back on USB.

2. After this, every subsequent fusgetstate over USB returned:
     FUS state is FUS_ERROR
     FUS status is FUS_NOT_RUNNING

3. Connected via ST-LINK (SWD, mode=HOTPLUG). -ob displ shows a
   stable, self-consistent option byte set (not SFSA=0x00, so
   safeboot/lock does not appear to have triggered):

     RDP     : 0xAA (Level 0, no protection)
     nBOOT0  : 0x1
     nBOOT1  : 0x1
     nSWBOOT0: 0x1 (later changed to 0x0 by repeated CLI FUS-operator
               writes -- each fusgetstate/fwupgrade/fwdelete call sets
               this itself as part of its internal routine)
     ESE     : 0x1 (Security enabled)
     SFSA    : 0xEC  (0x80EC000)
     FSD     : 0x0
     DDS     : 0x1
     C2OPT   : 0x1
     SBRV    : 0x3D000  (matches AN5185's documented "FUS v1.x/v2.x
               running" value, not the 0x3D800 v0.5.3 value)

   This SBRV/SFSA combination persisted unchanged through every step
   below.

4. Performed a full chip erase (unprotected user flash only, below
   SFSA) and a full power cycle (ST-Link fully unplugged, H3/BOOT0
   jumper to 3.3V to force bootloader, then USB plugged in). Flash at
   0x08000000 confirmed erased (all FFFFFFFF). Device info table:

     0x20030000 : 20030024 00000000 00000000 2003005C
     0x20030010 : 2003017C 00000000 00000000 00000000
     0x20030020 : 00000000 00000000 00000000 00000000
     0x20030030 : 00000000 00000000 00000000 00000000

   Table pointer (0x20030024) is present and correct per AN5185, but
   the FUS version word at 0x20030030 is all zeros. fusgetstate still
   returns FUS_ERROR / FUS_NOT_RUNNING at this point (over USB).

5. Tried stm32wb5x_FUS_fw.bin (latest, v2.2.0) via -fwupgrade over
   SWD with automatic address determination. Tool computed
   0x080E6000, erased/wrote/verified the image successfully
   ("Download verified successfully"), but the FUS itself then
   rejected the actual upgrade:

     Firmware Upgrade process started ...
     ...
     Error: FUS_STATE_ERR_UNKNOWN: Unknown error

6. Tried an RDP 0xAA -> 0xBB -> 0xAA cycle via -ob over SWD (per
   AN5185's FAQ recovery suggestion). Both transitions completed
   cleanly and reversibly; SFSA/SBRV unchanged throughout. No effect
   on FUS behavior.

7. Manually wrote PWR_CR4 to set C2BOOT and release CPU2, over SWD:

     STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -w32 0x5800040C 0x00008000

   This completed as a normal instant register write (no flash-style
   "Downloading..." banner, unlike writes to the flash controller's
   own registers e.g. 0x58004008 which the CLI routes through its
   flash-programming engine and which fail with "Failed to download
   data" on this chip in its current state).

   Afterward, fusgetstate was run 3x in a row over SWD per AN5185's
   FAQ recommendation ("ensures FUS is running and idle in most
   cases"):

     FUS_STATE_IDLE
     FUS_STATE_IDLE
     FUS_STATE_IDLE

   -ob displ immediately after: RDP=0xAA, SFSA=0xEC, SBRV=0x3D000 --
   unchanged.

   HOWEVER, the device info table read right after this (0x20030000,
   64 bytes, over SWD) still showed 0x20030030 = 00000000 (no FUS
   version populated), despite the GET_STATE calls succeeding.

8. Given the IDLE responses, tested an actual operation rather than
   just a status query, over SWD:

     STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -fwdelete

   Result:
     Error: FUS_STATE_ERR_UNKNOWN: Unknown error
     Firmware delete n°-17891602 failed after retrying!
     (retried 3x automatically, same result each time)

9. Re-ran -fwupgrade with stm32wb5x_FUS_fw_1_2_0.bin at 0x080EC000,
   firstinstall=0, over SWD, immediately after a fresh C2BOOT wake +
   3x confirmed FUS_STATE_IDLE. Same failure:

     Old wireless stack delete ...
     ...
     Error: FUS_STATE_ERR_UNKNOWN: Unknown error
     Error:
     Old Firmware delete failed

10. INTERFACE DISCREPANCY (confirmed, not a timing artifact):
    fusgetstate over SWD consistently returns FUS_STATE_IDLE,
    including when run as the very first command of a session with
    no prior C2BOOT write or any other command beforehand (tested
    cold specifically to rule out session-timing/wake-proximity
    effects). fusgetstate over native USB DFU (port=usb1, H3 held
    high) consistently returns FUS_ERROR / FUS_NOT_RUNNING, likewise
    as a cold first command, on the same chip, with no option byte
    changes in between sessions. However, on both interfaces, every
    actual operation (fwdelete, fwupgrade) still fails identically
    with FUS_STATE_ERR_UNKNOWN -- GET_STATE succeeding over SWD has
    not corresponded to operations actually working.

QUESTIONS

1. What does FUS_STATE_ERR_UNKNOWN actually mean in this specific
   context -- GET_STATE succeeding (IDLE), but any real operation
   (fwdelete, fwupgrade, regardless of binary/address) failing the
   same way, on both SWD and USB DFU interfaces, both before and
   after a manual C2BOOT wake? AN5185 Table 16 lists this as "0xFF:
   Unknown error" with no further detail -- is there internal
   diagnostic info (e.g. via a debug UART, trace channel, or a
   specific register) that could narrow this down further?

2. The device info table at 0x20030030 stays at 0x00000000 even
   immediately after 3 consecutive FUS_STATE_IDLE responses over SWD.
   Per AN5185 Section 1.2, this table should be populated by FUS at
   startup if FUS is genuinely running. Does this mean GET_STATE can
   return IDLE from some other code path than the actual FUS, or is
   there a timing/reset issue where the table gets cleared (e.g. via
   SRAM2RST on each of the repeated internal resets the CLI performs
   per command) before it can be read back?

3. The SWD-vs-USB-DFU GET_STATE discrepancy in point 10 is confirmed
   and not explained by query timing (tested cold, no prior commands
   in-session, on both sides). What would cause FUS_GET_STATE
   specifically to answer differently depending on which bootloader
   interface issues it, when AN5185 documents SWD and USB DFU as
   equally valid paths to the same FUS?

4. Is this chip's CPU2/FUS region recoverable at this point through
   any further procedure, or does the pattern above (stable,
   self-consistent option bytes; no SFSA=0x00; GET_STATE sometimes
   answering; every real operation failing identically regardless of
   interface) match a known failure mode that's specifically
   unrecoverable?

Happy to provide full verbose (level 3) logs for any of the above
steps, or try any specific diagnostic command.

1 reply

ST Technical Moderator
Nov 10, 2026 9:41 AM UTC

Hello ​@STMecko and welcome to ST Community,

I advise you to follow the recommendation and FAQ in the “STM32WB Firmware Upgrade Service” wiki page: STM32WB Firmware Upgrade Service - stm32mcu

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks