Skip to main content
Graham1
Associate II
Mar 17, 2025 4:39 PM UTC
Question

STM32WB55 disconnection issues after updating BLE binary to 1.21.0 from 1.20.0 when configured as both a central and peripheral

We have a device which connects to two other devices as a central, and also is connected to by a third device (Mobile Phone) as a peripheral.

When updating the Bluetooth firmware binary from version 1.20.0 to 1.21.0 we have started experiencing disconnections from the third device, downgrading back to 1.20.0 resolves any issues.

A summary of the connection flow is detailed below:

  • Device A (Peripheral) and Device B (Peripheral) are scanned for and connected to by Device C (Central)
  • Device C (Peripheral) Advertises and is scanned for and connected to by Device D (Central)
  • Device C soon stops responding to Device D and a connection timeout occurs (this is seen on wireshark and is not always the same point in the connection)

This behaviour is not observed, and the connection seems to be stable when Device C only connects to one of Device A or B before connecting to Device D, it also seems stable if the following sequence is performed:

  • Device A or B (Peripheral) connected to Device C (Central)
  • Device C (Peripheral) connected to Device D (Central)
  • Device B or A (Peripheral) connected to Device C (Central)
  • Device C can then be disconnected from Device D and reconnected manually without any timeout issues.

This suggests to me that it relates to the order in which devices are connected, however there could be other factors.

Has anyone else experienced anything similar, or got any suggestions on test I could perform to narrow down the cause.

Many Thanks, Graham

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Apr 9, 2025 5:22 PM UTC

Hello @Graham1 

Could you please give as more details (what you have received as logs, what are FWs that you are using, ...).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.