STM32WB55 Custom Board failing
- 6 replies
- 3022 views
Hey guys,
ive build a small custom pcb for the STM32WB55, much like the Usb Dongle (MB1293C, attatched schematic).
Without the µC the board is running fine, its mostly analog stuff + a 16 bit ADC for measuring strain gauges.
Even after having placed the µC and its bypass caps + oscillators, there are no issues.
As soon as i place the inductor (10µH) for its internal switch mode power supply, the board runs for 10-15 minutes. After that the 3V3 supply crashes and my switching regulator (MAX15062A) goes into hiccup mode, without being able to establish a constant supply voltage.
With no fault, powered down, GND to 3V3 rail resistance is about 100Ohms. After fault it goes down to about 5-10 Ohm. And it does not seem to recover after letting the board unpowered for a while.
My suspicion is that theres an internal short circuit inside the µC, apparently due to layout errors, although i tried to keep it close to the reference design of the usb dongle. But i cant seem to find them. Appreciate the help.