Skip to main content
AM.12
Associate III
Mar 2, 2023 6:19 AM UTC
Question

STM32WB55 custom board configured as Gatt Slave, after wateup from STOP2 mode UTIL_SEQ_SetTask and HW_TS_Start not working.

Case 1: without STOP2 mode UTIL_SEQ_SetTask or HW_TS_Start working fine.

Case 2: without UTIL_SEQ_SetTask or HW_TS_Start calling, the device can go to sleep and wake up without any problem.

case 3: when the device wakes up and after the device wakeup, if I use UTIL_SEQ_SetTask or HW_TS_Start device hangs up, and I am unable to debug also.

================Sleep code==========================

while (1)

 {

  /* USER CODE END WHILE */

  MX_APPE_Process();

  /* USER CODE BEGIN 3 */

  if(Go_TO_SLEEP)

  {

   Go_TO_SLEEP = false;

   HAL_GPIO_WritePin(MY_LED_GPIO_Port, MY_LED_Pin,1);

   HAL_Delay(5000);

   HAL_GPIO_WritePin(MY_LED_GPIO_Port, MY_LED_Pin,0);

    GPIO_InitStructure.Pin = GPIO_PIN_All;

    GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;

    GPIO_InitStructure.Pull = GPIO_NOPULL;

 //   HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);

 //     HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);

    HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);

    HAL_GPIO_Init(GPIOD, &GPIO_InitStructure);

    HAL_GPIO_Init(GPIOE, &GPIO_InitStructure);

    HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);

 //   __HAL_RCC_GPIOA_CLK_DISABLE();

 //      __HAL_RCC_GPIOB_CLK_DISABLE();

     __HAL_RCC_GPIOC_CLK_DISABLE();

     __HAL_RCC_GPIOD_CLK_DISABLE();

     __HAL_RCC_GPIOE_CLK_DISABLE();

     __HAL_RCC_GPIOH_CLK_DISABLE();

     DBGMCU->CR = 0;

    HAL_SuspendTick();

    LL_C2_PWR_SetPowerMode(LL_PWR_MODE_STOP2);

    HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

  }

=================================================================

==============EXTI Wakeup code===============================

 void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

 {

 SystemClock_Config();

  HAL_ResumeTick();

  UTIL_SEQ_SetTask(1 << CFG_TASK_ISR_CALLBACK, CFG_SCH_PRIO_0);

HAL_GPIO_WritePin(MY_LED_GPIO_Port, MY_LED_Pin,1);

Go_TO_SLEEP = true;

 }

==========================================

Without sleep modes my implementation works fine, when i use sleep modes, once device wakeup's not able to use UTIL_SEQ_SetTask or HW_TS_Start.

Can someone please help me with my problem

Thank you,

This topic has been closed for replies.

1 reply

Remy ISSALYS
ST Technical Moderator
Apr 21, 2023 4:23 PM UTC

Hello,

You can look BLE_HeartRate example available in STM32CubeWB package that allow to perform stop2 low power mode using low power manager.

Best Regards