Skip to main content
Ruubruben
Associate
May 6, 2022
Solved

STM32WB55 color control cluster gives an assertion error. assertion "zigbee_app_info.colorControl_server_2 != NULL" failed.

As I said, I get the assertion "zigbee_app_info.colorControl_server_2 != NULL" failed error from a standard debug function in the code.

I thought it could have something to do with this struct, which is a bit above it.

struct ZbColorClusterConfig colorServerConfig_2 = {
 .callbacks = ColorServerCallbacks_2,
 .capabilities = ZCL_COLOR_CAP_HS,
}

I feel like it has to be something I have to add here because this struct is checked to be NULL, but I can't seem to find what it is I have to add.

The place where the struct is set to something other than NULL is here:

zigbee_app_info.colorControl_server_2 = ZbZclColorServerAlloc(zigbee_app_info.zb, SW2_ENDPOINT, zigbee_app_info.onOff_server_2, NULL, 0, &colorServerConfig_2, NULL);

From what I could gather, this would allocate the space needed, but I guess something goes wrong and no memory is allocated.

This error occurs every time I start a new project and add the color control cluster. So it happens even when I haven't added anything.

This topic has been closed for replies.
Ruubruben
RuubrubenBest answer
Associate
May 10, 2022

So If anyone is also like me stuck here, the problem was the capabilities.

The code for it should be:

.capabilities = ZCL_COLOR_CAP_XY,

This is the only way I found to get it working, I don't know what the other capabilities are for.

At least I solved it : )

1 reply

Ruubruben
RuubrubenAuthorBest answer
Associate
May 10, 2022

So If anyone is also like me stuck here, the problem was the capabilities.

The code for it should be:

.capabilities = ZCL_COLOR_CAP_XY,

This is the only way I found to get it working, I don't know what the other capabilities are for.

At least I solved it : )