Skip to main content
Associate II
Apr 4, 2025 7:47 PM UTC
Question

STM32WB55: BLE project with with sequencer does not work with FreeRTOS

Hello,

I have a project where I work with BLE from the STM32WB55 series. I did this project using both FreeRTOS and Seqeuncer. The code content is exactly the same. However, after I put the Sequencer firmware on the processor, when I put the FreeRTOS project, BLE does not start broadcasting. However, if I load the Sequencer project, it works. This happens especially when I load the Sequencer project and then load the FreeRTOS project.
Both projects normally work without problems.

I wanted to do a full memory erase to solve this problem, but it was not enough. If I reload the BLE firmware on CPU1 and load the FreeRTOS project on the processor, it works without problems.

Do you have any information about this issue? Is this problem normal?
I would be glad if you could help.

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
Apr 4, 2025 7:54 PM UTC

Hello @inancmert 

Have you tested the same behavior with both BLE_HeartRate and BLE_HeartRateFreeRTOS 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
inancmertAuthor
Associate II
Apr 6, 2025 1:39 PM UTC

Hello,
I tested it after you told me but such a situation did not occur.

STTwo-32
ST Technical Moderator
Apr 7, 2025 8:37 AM UTC

Hello @inancmert 

So, you should check your code based on FREERTOS. You may follow the recommendation of the attached document for a successful conversation between Sequencer and FREERTOS based programs.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.