Skip to main content
Micha Valach
Associate III
Aug 24, 2020 5:57 AM UTC
Question

STM32WB55 BLE OTA Transfer Rate issue, and How to improve it?

Hello,

I successfully able to download and run the BLE_OTA example (on WB55-Nucleo platform)

I had transfer the M4 FW file only, named: BLE_p2pServer_ota_reference.bin with the size of 33.6KB, The Total transfer time was: 42.02 Sec (on my Huawei p10 mobile running "ST BLE Sensor" mobile App. v4.7.1)

Meaning the Transfer Rate is less then 10Kbits/Sec

Please advise why the Transfer Rate is so slow? and what need to do in order to make it faster?

Thanks In Advance,

Micha

This topic has been closed for replies.

2 replies

Remi QUINTIN
ST Technical Moderator
Aug 24, 2020 9:45 AM UTC

Most of the mobiles have a fixed and limiting connection interval as Bluetooth parameters. so it is difficult to show the real OTA performances with a mobile.

I did the same experiment with my mobile (Samsung A5) and I get the download doe in 32.17s which is still a quite low bit rate compare to the expected max throughput.

You could try the CubeMonitor-RF tool that get a higher bitrate as the connection interval can be easily modified.

Micha Valach
Associate III
Aug 24, 2020 9:50 AM UTC

Remi,

Thanks A Lot for your prompt reply

Micha