Skip to main content
AFede.1
Visitor II
Oct 14, 2022 1:57 PM UTC
Question

stm32wb55 avoid exit from sleep mode with TIM2 is active

Hello everybody, I am working with a stm32wb55 and in my application I need to send the microcontroller to sleep for 5 second, wake up, perform some actions and go back to sleep.

I send the micro to sleeomode using the function  HAL_PWR_EnterSLEEPMode and then I use the RTC wakeup to exit the sleep mode.

However, I also need to trigger an external watchdog every 200ms, and to do this I set TIM2 to generate an interrupt every 200ms and send a pulse to the external watchdog.

The problem is that, due to the interrupt generated by TIM2, the system exits sleepmode every 200ms and I want to avoid that. ideally, I would like to send the micro to sleep and keep the TIM2 active without waking the system up.

Is there any way to do that?

Thank you.

This topic has been closed for replies.

1 reply

Remy ISSALYS
ST Technical Moderator
Oct 19, 2022 1:17 PM UTC

Hello,

Are you using the timer server and the low power manager as in STM32CubeWB example like in BLE_HeartRate? If you have an interrupt every 200 ms, the system will wake-up every 200 ms. Instead of using TIM2 to refresh the watchdog, maybe you can refresh it when you are in idle state or inside a task with a minor priority.

Best Regards