Skip to main content
Associate
Sep 15, 2025 12:53 PM UTC
Question

STM32WB55 advertising dynamic switch from just works / legacy pincode

Hi,
I need to implement the following behavior on a STM32WB55.

Upon a command, device must advertise in 2 different modes:

  • Just works. No bonding, connection is accepted without any authentication requirements. All characteristics can be read and written.
  • Legacy pincode. No bonding, a fixed pincode shall be required by the host at every connection.

To acheive that, I followed scrupulously the ST wiki & configured the following:

  • aci_gap_set_io_capability
  • aci_gap_set_authentication_requirement
  • characteristic security permissions

I am able to have either one of the 2 scenarii, but I cannot switch dynamically from one another.


The key difference resides in the security permission of each characteristic.

  • With ATTR_PERMISSION_NONE, characteristics can be read & written without authentication (just works mode)
  • With ATTR_PERMISSION_AUTHEN_READ | ATTR_PERMISSION_AUTHEN_WRITE, pincode is properly required at each connection.

Unfortunately, I cannot switch dynamically between the 2.

I tried the following: 

  • A call to aci_gatt_set_access_permission. This returns 0x0C - command disallowed
  • I tried to telete all characteristics and re-create them calling aci_gatt_del_char and aci_gatt_add_char_desc but I have the error code 0x98 Out of memory.
    The stack fails to recreate the the last characteristic as if there was some king of memory leak in the stack (if called repeatedly, the last characteristic goes up in the creation loop ...)

Here are my questions:

  • Is there a way to achieve this without changing the permissions of the characteristics ?
  • If no, can I change the permissions dynamically ?
  • If no, do you think of any way that would not need deleting characteristics ?
  • If no, can ST investigate the possible memory leak at characteristic deletion ?

 

Code snippet of the authentication requirements:

 

 /**
 * Configuration that differs upon advertizing mode
 */
 switch (mode)
 {
 case ble_advertize_justworks:
 io_capability = IO_CAP_NO_INPUT_NO_OUTPUT;
 MITM_Mode = CFG_MITM_PROTECTION_NOT_REQUIRED;
 break;
 case ble_advertize_passkey:
 io_capability = IO_CAP_DISPLAY_ONLY;
 MITM_Mode = CFG_MITM_PROTECTION_REQUIRED;
 break;
 default:
 assert(FALSE); // should not reach here
 break;
 }

 /**
 * Set I/O capability
 */
 ret = aci_gap_set_io_capability(io_capability);
 if (ret != BLE_STATUS_SUCCESS) {
 APP_DBG_MSG("aci_gap_set_io_capability failed with status %x", ret);
 return ret;
 }
 /**
 * Configure authentication
 */
 ret = aci_gap_set_authentication_requirement(0, // No bonding required
 MITM_Mode,
 CFG_SECURE_NOT_SUPPORTED,
 CFG_KEYPRESS_NOT_SUPPORTED,
 CFG_ENCRYPTION_KEY_SIZE_MIN,
 CFG_ENCRYPTION_KEY_SIZE_MAX,
 0, // use a fixed pin
 passkey, // fixed pin value
 GAP_PUBLIC_ADDR); // identity address type
 if (ret != BLE_STATUS_SUCCESS)
 {
 APP_DBG_MSG("aci_gap_set_authentication_requirement failed with status %x", ret);
 return ret;
 }

 /**
 * Fill UUID with UUID
 */
 memcpy(&(ble_adv_uuid[1]), ble_get_uuid(), sizeof(ble_uuid_t));

 /**
 * Start advertising
 */
 ret = aci_gap_set_discoverable(
 ADV_IND,
 CFG_FAST_CONN_ADV_INTERVAL_MIN,
 CFG_FAST_CONN_ADV_INTERVAL_MAX,
 BLE_ADDR_TYPE,
 NO_WHITE_LIST_USE,
 sizeof(ble_local_name) - 1, /* Don't count the 0 byte at the end */
 (uint8_t*) ble_local_name,
 sizeof(ble_adv_uuid),
 (uint8_t*) ble_adv_uuid,
 0, /* No specific minimum connection interval */
 0 /* No specific maximum connection interval */
 );
 if (ret != BLE_STATUS_SUCCESS) {
 APP_DBG_MSG("aci_gap_set_discoverable failed with status %x", ret);
 return ret;
 }

 

11 replies

ST Employee
Sep 16, 2025 11:27 AM UTC

Hello @lgrosbois_WTK,

to your questions:

1) no, you have to change the permissions of characteristics according to your need in terms of security. If security permissions of the characteristic will be higher than link security level, characteristic won't be accessible. So you may need to change characteristic security permissions

2) aci_gat_set_access_permission and aci_gat_set_security_permission, can change security properties only of attributes, not entire characteristics

3) My idea is if it could be sufficient for you that you would have no_init variable and when you want to change the mode, you would change this variable and perform NVIC_System_Reset. Then you would set security requirements according to this variable

4) I would probably need your logs and your steps to the deletion and adding of characteristic in order to replicate your issue

 

 

Associate
Sep 22, 2025 7:15 AM UTC

Hello @grohmano ,

My customer is OK for me spending time on this issue.
Although, I cannot send you his code.


I will modify the ble_heartrate example in order to reproduce my issue and provide you with it.

hope I will w be able to send you something within the 2 coming weeks.

 

Kind regards,

Laurent

 

Associate
Sep 16, 2025 12:15 PM UTC

Hello @grohmano,

Thank you for your reply.

As I understand, I need either to:

- fix what looks like a memory leak in the stack

- perform a hard reset of the chip

 

Reset is not an option, as the WB55 features is not only performing BLE, but also has other tasks in active use.

I will see during the week what I can provide you with in order to reproduce the issue.


FYI, I am using stm32wb5x_BLE_Stack_full_fw.bin, version STM32Cube_FW_WB_V1.20.0.
I checked with the latest release note and there is no mention of fixing a memory leak in the changelog.

Kind regards,

Associate
Nov 18, 2025 7:57 PM UTC

Dear @grohmano ,

I finally found the time to work on a PoC to reproduce the issue.

Please find enclosed a modified ble_heartrate:

- A new BLE service with numerous characteristics replaces the usual services which have been commented out

- Logs have been enabled

- Gatt configuration variables have been modified (CFG_BLE_NUM_GATT_SERVICES, CFG_BLE_NUM_GATT_ATTRIBUTES, CFG_BLE_ATT_VALUE_ARRAY_SIZE).
- Button switch 1 function has been modified to trigger characteristic deletion / re-creation

- I did not port event handling as I did not thinbk it was relevant to the issue reproduction. 

 

As you will see, service and characteristics instanciation are fine at init.
When pressing switch1, service and characteristics are deleted. Then, the last characteristic cannot be instanciated due to lack of memory. When re-trying, then characteristic n-2 cannot be instanciated, and so on with n-3, ...

Please see the logs below.

 

==>> Start Ble_Hci_Gap_Gatt_Init function
 Success: hci_reset command
 Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
 Public Bluetooth Address: 00:80:e1:26:c1:c3
 Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET
 Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET
 Success: aci_hal_set_tx_power_level command
 Success: aci_gatt_init command
 Success: aci_gap_init command
 Success: aci_gatt_update_char_value - Device Name
 Success: aci_gatt_update_char_value - Appearance
 Success: hci_le_set_default_phy command
 Success: aci_gap_set_io_capability command
 Success: aci_gap_set_authentication_requirement command
 Success: aci_gap_configure_whitelist command
==>> End Ble_Hci_Gap_Gatt_Init function

[BLE] Create service success
[BLE] Create characteristic success
==>> aci_gap_set_discoverable - Success
==>> Success: Start Fast Advertising

==>> BUTTON 1 pressed
[BLE] Delete characteristic success
[BLE] Delete service success
[BLE] Create service success
[BLE] Failed to create characteristic 0x0074: error 0x0098
==>> BUTTON 1 pressed
[BLE] Delete characteristic success
[BLE] Delete service success
[BLE] Create service success
[BLE] Failed to create characteristic 0x0073: error 0x0098
==>> BUTTON 1 pressed
[BLE] Delete characteristic success
[BLE] Delete service success
[BLE] Create service success
[BLE] Failed to create characteristic 0x0071: error 0x0098
==>> BUTTON 1 pressed
[BLE] Delete characteristic success
[BLE] Delete service success
[BLE] Create service success
[BLE] Failed to create characteristic 0x0071: error 0x0098
==>> BUTTON 1 pressed
[BLE] Delete characteristic success
[BLE] Delete service success
[BLE] Create service success
[BLE] Failed to create characteristic 0x0070: error 0x0098
==>> BUTTON 1 pressed
[BLE] Delete characteristic success
[BLE] Delete service success
[BLE] Create service success
[BLE] Failed to create characteristic 0x0060: error 0x0098

 

ST Employee
Nov 19, 2025 1:38 PM UTC

Hello @lgrosbois_WTK,

I have replicated the issue but did not find the cause, so I have submitted a ticket to our developers for verification and will let you know when I know more.

Best regards

Associate
Nov 20, 2025 7:50 AM UTC

Hello @grohmano ,

 

Wow, that was fast ! Thanks !

Please keep me posted :).
Have a nice day,

 

Laurent

Associate
Dec 3, 2025 10:08 AM UTC

Hello @grohmano ,

 

Any update from ST development team ?

 

Thanks !

ST Employee
Dec 3, 2025 10:18 AM UTC

Hello,

no, not yet. We can expect some update in January probably.

Sorry for the delay 

Lubos KOUDELKA
ST Employee
Dec 16, 2025 2:13 PM UTC

Dear @lgrosbois_WTK ,
we got feedback from development team - issue was found in address calculation when characteristic with a CCCD is deleted. Will be fixed in new release.
Checking for possible workaround now, aci_gatt_set_security_permission shall do the job here as well.

Trying in your project to change in ta_ble_delete_characteristics function

//status = aci_gatt_del_char (ta8x_service_handle, ch->handle);
status = aci_gatt_set_security_permission(ta8x_service_handle, (ch->handle)+1, 0x4);

and comment out all delete functions

 ta_ble_delete_characteristics();
// ta_ble_delete_service();
// ta_ble_create_service();
// ta_ble_create_characteristics(security_permissions);

Read access to characteristic requires encryption, there is need for pairing when you read such characteristic from client.
Please check also on your side.

Best regards,
Lubos

 

Associate
Dec 16, 2025 3:21 PM UTC

Dear @Lubos KOUDELKA ,

 

Great news, thanks for your reply !

 

Regarding the workround, I am surprised as @grohmano stated the following on  ‎2025-09-16 4:27 AM.

Has this been changed in recent versions ?

 


2) aci_gat_set_access_permission and aci_gat_set_security_permission, can change security properties only of attributes, not entire characteristics


Lubos KOUDELKA
ST Employee
Dec 16, 2025 3:42 PM UTC

No it was not changed in recent version, but we clarified correctly with development the functionality and possible usage