Solved
STM32WB55 - ACI_HAL_TONE_START command rf channel resolution
Hi everyone,
I use STM32WB55 with the BLE stack 13.0 (full version) and want to test the RF. In the an5270 document, I noticed the ACI_HAL_TONE_START command and it is allowed to change the rf channel from 2.402 to 2.480 GHz with 2 MHz resolution. However, I want to change the channel to a 1 MHz resolution. For example, I want to set the channel to 2.403 GHz. Is it possible to do? If yes, how?
Thank you.
Have a nice day.
Serhat.