STM32WB1x BLE Full Extended Stack V1.25.0 – USART DMA streaming issue
Hello ST team,
I am using the B-WB1M-WPAN1 (STM32WB1MMC) board with the BLE Full Extended Stack.
My application is based on BLE_DataThroughput and operates as a bridge between an STM32G473 and a smartphone.
Data can be transferred from the STM32G473 to the STM32WB1MMC using either USART1 DMA or SPI DMA, and then forwarded through BLE notifications (244 data bytes + CRC8).
The application works correctly with STM32Cube_FW_WB V1.24.0 and its BLE stack.
After updating the STM32WB1x BLE Full Extended Stack to the version supplied with STM32Cube_FW_WB V1.25.0, I observed the following:
-
Both SPI transmission modes continue to work.
-
USART1 DMA streaming no longer works correctly.
-
BLE advertising, connection, initial handshake and commands from the smartphone still work.
-
USART1, DMA1 and DMAMUX registers appear correctly configured.
-
Increasing
CFG_TLBLE_EVT_QUEUE_LENGTHfrom 5 to 10 did not resolve the issue.
I also tested the original working V1.24.0 application without modifying its source code, using the new V1.25.0 wireless stack. The result was the same: SPI worked, but USART streaming did not.
My question:
Are there any changes in the STM32WB1x BLE Full Extended Stack between V1.24.0 and V1.25.0 that require modifications to CPU1 application initialization, BLE event handling, transport-layer buffers, or notification processing?
I am particularly interested in changes specific to the STM32WB1x binary stack, rather than STM32WB55.
Thank you for your assistance.