Skip to main content
Associate
Aug 26, 2025 6:41 AM UTC
Question

STM32WB1MMCH OTP

STM32WB1MMCH:Can other values be written again after the otp area is written to 0xFF

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
Aug 26, 2025 7:56 AM UTC

Hello @luzuhua and welcome to the ST Community.

According to the RM0473,

« 1 Kbyte (128 double words) OTP (one-time programmable) for user data. The OTP data cannot be erased and can be written only once. If only one bit is at 0 the entire double word (64 bits) cannot be written anymore, even with the value 0x0000 0000 0000 0000. »

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
luzuhuaAuthor
Associate
Aug 26, 2025 8:57 AM UTC

The first time I write 0x5a to 0x1FFF7008-0x1FFF70F7,and other addr i write 0xFF;The second time,i want to write some value to 0x1FFF70F8-0x0x1FFF73F7,but I found that I cannot write it,May I ask why this is?

STTwo-32
ST Technical Moderator
Sep 23, 2025 4:21 PM UTC

As i mentioned before, The OTP data cannot be erased and can be written only once. This should be the explication of the behavior you are having here.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.