Skip to main content
Visitor II
Sep 2, 2025 4:34 AM UTC
Question

STM32WB1MMC external antenna design support and calculation solution

I have previously worked on a BLE-based application that required an external antenna. Based on the use case, I selected the STM32WB1MMC module, which, according to its datasheet, supports external antenna connections. I designed the schematic accordingly and initially conducted tests using the internal antenna. After validating the basic functionality, I transitioned to testing with the external antenna as per the actual use case requirements. I obtained this information from "

External antenna interface is only verified for conducted testing. Device has been verified and tested with internal antenna."

jvcmani_0-1756786632274.png

 

Based on the information provided in the datasheet, can we proceed with using the module's external SMA antenna connection? Do I need to perform any calculations for a Pi matching circuit or conduct further fine-tuning? Additionally, could you suggest any reference designs or recommended external antenna configurations suitable for this module?"

 

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Sep 26, 2025 8:20 AM UTC

Hello @jvcmani 

The Certification is done using the internal antenna. So, the values done throw the internal antenna may be used as a reference, but it may not be exactly the same. For reference design, you may have a look at the B-WB1M-WPAN1 and the chapter 9 of the AN5165 as a reference for your design.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.