Solved
Stm32wb15ccu i2c bus never has signal edges
I design a custom board including a stm32wb15ccu where I want to use the I2C bus. I have for SDA and SCL 10k pull up resistors. However when launching i2c the signal of SDA and SCL remain at 3.3V, no bus signal. Hence I could not communicate between the MCU and its slaves. pin 5 is SCL and pin 6 is SDA.
What I did so far to get the cause:
- Connected an external nucleo to the i2c pin headers , this worked perfectly fine.
- Resoldered the MCU chip multiple times
- Desoldered the pull up resistors, if somewhere 3V3 is shorted to the i2c. What I found interesting when desoldered the pull up resistors the voltage of the i2c is still at 0.2V instead of zero.
What I suppose a possible cause:
- Partly damage of the MCU
- Design error, wrong pin selected for I2C on the WB
TThanks in advance for any help