Skip to main content
LConn.2
Associate
Mar 20, 2023 3:52 PM UTC
Question

STM32WB15cc - Wake up periodically with RTC and check for event (battery charged), disable rtc if event has happened

I am trying to use as little power as possible, I want my board to wake up every 30 seconds or so, check if battery has been sufficiently charged, if not, go back to sleep, if it has then turn off rtc and do a function. Is it possible to disable rtc whilst running?

This topic has been closed for replies.

4 replies

Joe WILLIAMS
ST Employee
Mar 22, 2023 2:15 AM UTC

Dear Liam

Our team is checking into this inquiry and we will be in touch with you shortly.

Kind Regards

Joe WILLIAMS

STMicro Support

Piranha
Principal III
Mar 22, 2023 6:14 PM UTC

> Is it possible to disable rtc whilst running?

What makes you think the RTCEN bit in RCC_BDCR register cannot be cleared?

Remy ISSALYS
ST Technical Moderator
Mar 31, 2023 2:26 PM UTC

Hello,

You can disable the RTC by setting the RTCSEL in RCC_BDCR register at no clock.

Best Regards

Piranha
Principal III
Apr 1, 2023 9:34 AM UTC

Bits 9:8 RTCSEL[1:0]: RTC clock source selection

Set by software to select the clock source for the RTC. Once the RTC clock source has been selected, it cannot be changed anymore unless the Backup domain is reset, or unless a failure is detected on LSE (LSECSSD is set). The BDRST bit can be used to reset them.