Skip to main content
Davide Dalfra
Associate III
May 9, 2025 4:38 PM UTC
Question

STM32WB09KE PAwR Setting Maximum Connection Interval

Hello Folks,

 

I started playing with STM32WB09 after some difficulties related to entering in bootloader mode (thanks again to the community) and i wanted to try setting the maximum SCAN_INTERVAL + maximum CONNECTION_INTERVAL to see the best low power footprint i can obtain.

All the setting i'm playing with are in app.conf.h and are basically those:

#define PAWR_NUM_SUBEVENTS 4
#define PAWR_SUBEVENT_INTERVAL_MS 30
#define PAWR_RESPONSE_SLOT_DELAY_MS 2.5
#define PAWR_RESPONSE_SLOT_SPACING_US 500
#define PAWR_NUM_RESPONSE_SLOTS 8

#define PAWR_INTERVAL_MS (PAWR_SUBEVENT_INTERVAL_MS * PAWR_NUM_SUBEVENTS + 200)
 
#define SCAN_INTERVAL_MS 2000
#define SCAN_WINDOW_MS 100
#define CONNECTION_INTERVAL_MS 200
#define SUPERVISION_TIMEOUT_MS 500

 

Strating from the Broadcaster example, i'm able to set the maximum "SCAN_INTERVAL_MS" up to 32000ms (32s).
I can see that from the power consumption footprint the system wake up every 32s scanning for observers.

However i'm getting a strange behavior while changing the CONNECTION_INTERVAL_MS.
The maximum working value i obtained experimentally is 200 or lower. 

The call where this defines is used, to configure the lower hardware level is in app.ble.c

status = aci_gap_set_connection_configuration(LE_1M_PHY_BIT,
 (CONNECTION_INTERVAL_MS*100)/125, (CONNECTION_INTERVAL_MS*100)/125,
 0u,
 SUPERVISION_TIMEOUT_MS/10,
 2, 2); 

 if (status == BLE_STATUS_SUCCESS)
 {
 APP_DBG_MSG("==>> aci_gap_set_connection_configuration Success , result: 0x%02x\n", status);
 }
 else
 {
 APP_DBG_MSG("==>> aci_gap_set_connection_configuration Failed , result: 0x%02x\n", status);
 Error_Handler();
 } 

As per AN6142 the maximum value configurable on this call, for "Connection_Interval_Min" and "Connection_Interval_Max" is 0x0C80  (corresponding to 4s).

DavideDalfra_0-1746808467748.png

Even by setting raw values on the aci_gap_set_connection_configuration, nothing changes as i always get correct return values (0x00) ;however the next call which is to aci_gap_start_procedure failed with return code 0x12.

status = aci_gap_start_procedure(GAP_AUTO_CONNECTION_ESTABLISHMENT_PROC, LE_1M_PHY_BIT, 0, 0);
 if (status != BLE_STATUS_SUCCESS)
 {
 APP_DBG_MSG("aci_gap_start_procedure - fail, result: 0x%02X\n", status);
 Error_Handler();
 }
 else
 {
 APP_DBG_MSG("==>> aci_gap_start_procedure (auto connection) - Success\n");
 } 

UART Debug is as follows:

SYSTEM RESET!!!!!!!!!<LF>
<LF>
 Success: aci_hal_set_tx_power_level command<LF>
 Success: aci_gatt_srv_profile_init command<LF>
 Success: aci_gap_init command<LF>
 Static Random Bluetooth Address: e5:f9:53:f8:b3:22<LF>
 Success: Gap_profile_set_dev_name - Device Name<LF>
 Success: Gap_profile_set_appearance - Appearance<LF>
 Success: aci_gap_set_io_capability command<LF>
 Success: aci_gap_set_security_requirements command<LF>
 Success: aci_gap_configure_filter_accept_and_resolving_list command<LF>
 Success: aci_gap_set_le_event_mask command<LF>
==>> End BLE_Init function<LF>
==>> Success: aci_gap_set_advertising_configuration<LF>
==>> Success: hci_le_set_periodic_advertising_parameters_v2<LF>
==>> Success: hci_le_set_periodic_advertising_enable<LF>
==>> Success: hci_le_set_extended_advertising_enable<LF>
==>> aci_gap_add_devices_to_filter_accept_and_resolving_list - Success<LF>
==>> aci_gap_set_scan_configuration - Success<LF>
==>> aci_gap_set_connection_configuration Success , result: 0x00<LF>
aci_gap_start_procedure - fail, result: 0x12<LF>
<LF>
<LF>
SYSTEM RESET!!!!!!!!!<LF>
<LF>
 Success: aci_hal_set_tx_power_level command<LF>
 Success: aci_gatt_srv_profile_init command<LF>
 Success: aci_gap_init command<LF>
 Static Random Bluetooth Address: e5:f9:53:f8:b3:22<LF>
 Success: Gap_profile_set_dev_name - Device Name<LF>
 Success: Gap_profile_set_appearance - Appearance<LF>
 Success: aci_gap_set_io_capability command<LF>
 Success: aci_gap_set_security_requirements command<LF>
 Success: aci_gap_configure_filter_accept_and_resolving_list command<LF>
 Success: aci_gap_set_le_event_mask command<LF>
==>> End BLE_Init function<LF>
==>> Success: aci_gap_set_advertising_configuration<LF>
==>> Success: hci_le_set_periodic_advertising_parameters_v2<LF>
==>> Success: hci_le_set_periodic_advertising_enable<LF>
==>> Success: hci_le_set_extended_advertising_enable<LF>
==>> aci_gap_add_devices_to_filter_accept_and_resolving_list - Success<LF>
==>> aci_gap_set_scan_configuration - Success<LF>
==>> aci_gap_set_connection_configuration Success , result: 0x00<LF>
aci_gap_start_procedure - fail, result: 0x12<LF>
<LF>
<LF>
SYSTEM RESET!!!!!!!!!<LF>



Anyone already encountered similar problem?

 

Regards

Davide

 



This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
Jun 20, 2025 10:26 AM UTC

Hello @Davide Dalfra 

This behavior has been escalated internally (under internal ticket number 212654) and i will be back to you ASAP.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Davide Dalfra
Associate III
Jul 6, 2025 7:25 AM UTC

Hello,

 

Thanks. Any news on that?

 

 

D.

STTwo-32
ST Technical Moderator
Aug 1, 2025 9:15 AM UTC

Hello @Davide Dalfra 

If connection interval is changed, supervision timeout may also need to be changed. This is the description of Supervision_Timeout: The Supervision_Timeout in milliseconds shall be larger than (1 + Max_Latency) × Connection_Interval_Max × 2, where Connection_Interval_Max is given in milliseconds.

So, to be able to attend the maximum level of the Connection_Interval_Max, you need to set the Supervision_Timeout to the maximum value as indicated on the chapter 2.4.26 of the AN6182.

 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.