Skip to main content
Visitor II
Sep 2, 2026 10:31 AM UTC
Question

STM32WB06 low-power issue with BLE auto connection

Hi, I'm having some issues with the STM32WB06 when trying to achieve low power consumption. I hope someone can help me solve these problems.

Issue 1: After initializing the Bluetooth protocol stack and enabling automatic connection establishment, it causes the device to fail to enter the low power state (BLE wake-up has been disabled). Is this a normal phenomenon? If not, what are the solutions?

Issue 2: Before entering the low power mode, disabling automatic connection establishment allows the device to enter the low power mode normally. However, after waking up, attempting to re-enable automatic connection establishment fails (aci_gap_start_procedure(GAP_AUTO_CONNECTION_ESTABLISHMENT_PROC, LE_1M_PHY_BIT, 0, 0)). What is the solution for this problem?

b55459cd-ab05-8509-7671-423bbaeadb7d.png

 

I look forward to your replies. Thank you very much!

1 reply

ST Technical Moderator
Sep 27, 2026 7:37 PM UTC

Hello ​@xxyyhhmm and welcome to the Community,

Thanks for your patience.

I consulted our Wireless team, and they answered the following:

Autoconnection establishment procedure consists in scanning for devices. The ability to enter low power states depends on the duty cycle. If the duty cycle is near 100 %, the device cannot enter deepstop mode. The device can use deepstop mode between scan windows only if there is enough time (i.e. more than 2-3 ms).

Regarding the issue with the restart of the procedure, we need to know the complete sequence of commands.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks