Skip to main content
Associate II
Feb 18, 2025 3:54 AM UTC
Solved

STM32WB05KN co-processor USART is not responding (bluetooth)

Hello, hope someone can help me, thx!

 

I successfully completed the SensorDemo_BLESensor-App by connecting NUCLEOWB05KN1 with NUCLEO-U575ZI-Q, and carefully followed the manual X-CUBE-WB05N_GettingStarted. I have also verified that we can send data by Bluetooth on NUCLEOWB05KN by only connecting the VDD, GND, and the RX, TX to the TX and RX of the NUCLEO-U575ZI-Q. 


However, we built a PCB that exactly copy from stdes-wb05kv2ld (two-layer board), and assembled the stm32wb05kn and the components (same as stdes-wb05kv2ld) onto the PCB. When we connected the PCB with NUCLEO-U575ZI-Q by 3V3, GND, RX to PCB's USART TX, and TX to PCB's USART RX, the WB05KN is not responding; by the logic analyzer, we can see that the NUCLEO-U575ZI' TX is sending out the data, but stm32wb05kn is not responding; it remains logic high.

 

I was thinking if the chip has been lock-up accidentally, so we have also tried the stm32programmer, by connecting the swdio, swclk, NRST, 3V3 and GND to st-link, the stm32programmer said that no device connected, but thestm32programmer can recognize the NUCLEOWB05KN1.

 

Meanwhile, using an oscilloscope, we can see the SMPS. There is a high-frequency voltage feeding the VFBSD pin. The multimeter verified that all the connections were connected.

So, for the STM32WB05KN co-processor, we can just use the NUCLEO-U575ZI-Q default example (SensorDemo_BLESensor-App) setting to communicate with it by USART without any other settings(like updating the firmware, an extra event to wake-up the chip rather than the start pulse...), right?

And is there anything we should check? Or do you think the chip accidentally died?

 

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 20, 2025 5:43 PM UTC

Hello @Harry_bee 

This is normal since the X-NUCLEO-WB05KN1 contain a firmware that configure the shield to communicate with a Host. Without a similar FW, you design is a board and not a module controlled by a Host. The firmware of the X-NUCLEO-WB05KN1 is available under Utilities\DTM_Controller_Only on the X-Cube-WB05N. 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 20, 2025 5:43 PM UTC

Hello @Harry_bee 

This is normal since the X-NUCLEO-WB05KN1 contain a firmware that configure the shield to communicate with a Host. Without a similar FW, you design is a board and not a module controlled by a Host. The firmware of the X-NUCLEO-WB05KN1 is available under Utilities\DTM_Controller_Only on the X-Cube-WB05N. 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Harry_beeAuthor
Associate II
Feb 21, 2025 1:33 AM UTC

Hi STTwo-32,


Thanks for your insightful information. I will try to assemble a new board with this chip to rule out the bad chip assumption first, and I will try to upload the DTM_UART_WITH_UPDATER_CONTROLLER.hex in the Utilities\DTM_Controller_Only path by STM32CubeProgrammer.

  • And for another issue I demonstrated here before:

    ---''by connecting the swdio, swclk, NRST, 3V3 and GND to st-link, the stm32programmer said that no device connected, but the stm32programmer can recognize the NUCLEOWB05KN1 with same connection"

    Do you have any further suggestions? Do I need to do anything else to "wake up" the new chip without firmware yet, or do you think this could be only about the connection or bad chip issue?  I have connected the NRST to 3V3 with 10k and to GND as well with a 0.1uf capacitor.

Thanks again for your help and support!

Best,