Skip to main content
RAdam.1
Associate III
Jun 12, 2026 3:54 PM UTC
Question

STM32WB05 reboots when advertising starts ; Reposting

Reposting due to last topic vanishing during migration.

I have an project running great on a STM32WB05 nucleo platform. I have built my own custom board and everything works great until it starts to advertise and then it reboots.. I have double checked everything on the board and it matches the reference design. I am using the internal SMPS and running on a bench supply currently at 3.3V limited at 300mA

Looked at a bunch of things but really cant understand the issue. If i stop it advertising (change nothing else) then it starts up perfectly and runs. 

Other symptoms/info

Board is drawing 7mA which seems high for idle (no low power mode enabled yet). 

I had 4 boards made. One worked briefly on the PSU. I then used a coin cell and it starting failing on that. Now doesnt work on PSU.

Any sensible ideas welcome especially from anyone who has seen this. In many years of BLE development, i havent