Skip to main content
David Koster
Associate II
Apr 13, 2026 1:44 PM UTC
Question

STM32WB05 - 1.8V supply IOs, 3.3V pullups. Clamped at 2.5V?

I have a STM32WB05TZF6TR. All VCCs are running off 1.8V. I'm trying to use PA8 and PB5 with 3.3V 10k pullups. But the signals are being clamped at 2.5V. I had expected this not to happen, as they are supposed to be 5V tolerant. 

Does anyone know what's happening here? There's nothing connected to the pins besides the pullups. 


I have a bare STM32CubeMX project, with just this GPIO init:

void MX_GPIO_Init(void){
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /*Configure GPIO pin : PB5 */
 GPIO_InitStruct.Pin = GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : PA8 */
 GPIO_InitStruct.Pin = GPIO_PIN_8;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}

 
Much appreciated,
David 

4 replies

Peter BENSCH
ST Technical Moderator
Apr 14, 2026 8:20 AM UTC

A 5V tolerant pin does not mean it can be pulled to 3.3V in every mode and supply condition. With the chip powered at 1.8V, the pin is probably being clamped by its protection structure at about: VDD+0.6...0.8V = 2.4...2.6V. So your ~2.5V reading is expected. If you want to avoid that, you should use a level shifter or an input current limit set by a series resistor.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ozone
Principal
Apr 14, 2026 8:42 AM UTC

You beat me to it ...

This 2.5V - 1.8V difference looks a lot like the average VF (forward voltage) of a p-n junction, probably a protective diode.