Question
STM32WB Thread-RCP and Raspberry Pi 3B for Border Router feature.
From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says:
"This application is used to demonstrate the OpenThread Border router feature using an STM32WB device.
To play with the demo, you need a Raspberry Pi 3B (RPi) to perform the link with Wi-Fi/Ethernet networks
The full setup and the associated documentations can be requested to ST on demand".
Where can I find the full setup and associated documentation?
Thank you,