Skip to main content
DS.4
Senior
May 23, 2021 7:15 AM UTC
Question

STM32WB - PLACE_IN_SECTION

Looking at the HearRate Example with RTOS.

I see that user app holds all the handlers in :

PLACE_IN_SECTION("BLE_DRIVER_CONTEXT") static HRS_Context_t HRS_Context;

What is the purpose of this placement?

Can it be changed to a simple static?

thanks

This topic has been closed for replies.

2 replies

Remi QUINTIN
ST Technical Moderator
Jul 21, 2021 6:54 AM UTC

This section is not used anymore. We will remove those lines from the code.

The original idea was to identify all BLE contexts to record them in memory when using standby mode.

BBurc.1
Associate
Oct 21, 2021 7:27 AM UTC

Dear Sirs,

I am fighting with a similar problem: Inside hci_tlc.c these variables are declared and the program tries to catch data from  address 0x300cf810. "Cannot access memory at address 0x300cf810" is the exact error message. Since the variable "pCmdBuffer->cmdserial.cmd.cmdcode = opcode;" is used in proc "static void SendCmd(uint16_t opcode, uint8_t plen, void *param)" at line 243, this causes a program halt.

So, how to proceed to continue with coding?

BR Bernd