Skip to main content
SWenn.1
Senior III
Feb 24, 2024 12:54 AM UTC
Question

STM32WB Notification doesn't seem to be working?

Hello 

I am using the following to try and get a notification from an STM32WB Nucleo server to my phone the client but cannot get it to work.

BLE Notifications ---- ST Micro video 

I compile and can see the two characteristics on my phone but when I push the button on the board my phone never updates with anything.  I have tried ST Toolbox and nRF Connect and neither works.

I have attached my project pdf file from CubeMX.  This project was built on a test that does Pairing and Bonding with Pairing required only on certain characteristics from the Product service.  After this was working successfully I added the STATUS service (page 18) which is pretty similar to the video. 

The difference is the VALVE characteristic has permission set to:

ATTR_PERMISSION_AUTHEN_WRITE = YES

and GATT event set to :

GATT_NOTIFY_WRITE_REQ_AND_WAIT_FOR_APPL_RESP = YES

The second characteristic is the NOTIFICATION which the video is based off of (see page 18 of the pdf).

Can anyone please share some light as to what I might try?

Thank you

Steve

This topic has been closed for replies.

3 replies

Dsarychev
Visitor II
Mar 15, 2024 2:51 PM UTC

Hi,

Had the same issue for a week. In my case the "if" statement was the culprit. It is generated in a way, that it never executes the "Custom_Button_c_Update_Char" function.

In my case the name of the service is "myService" and the name of my characteristic is "Button_c"

Try to modify the generated code in the "custom_app.c" file like so:

 

/* myService */
void Custom_Button_c_Update_Char(void) /* Property Read */
{
uint8_t updateflag = 0;

/* USER CODE BEGIN Button_c_UC_1*/
Custom_STM_App_Update_Char(CUSTOM_STM_BUTTON_C, (uint8_t *)UpdateCharData);
/* USER CODE END Button_c_UC_1*/

if (updateflag != 0)
{
Custom_STM_App_Update_Char(CUSTOM_STM_BUTTON_C, (uint8_t *)UpdateCharData);
}

/* USER CODE BEGIN Button_c_UC_Last*/

/* USER CODE END Button_c_UC_Last*/
return;
}

This way you avoid code modification everytime you re-generate your code.

 

Also, I can't seem to find the attachment you mentioned.

STTwo-32
ST Technical Moderator
Apr 15, 2024 1:27 PM UTC

Hello @SWenn.1 

I suggest you take a look at this WIKI. It should be Helpful. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Yasin Yelkovan
Associate II
Apr 16, 2024 10:25 AM UTC

Hi SWenn,

I had the same problem with this video tutorial, so I made some changes and share them below:

 

 

** custom_app.c **
1)Add these variables: 
/* USER CODE BEGIN PV */
uint8_t notifyStatus = 0;
uint8_t button1Status = 0;
/* USER CODE END PV */

2) Modify the fuction:
/* USER CODE BEGIN PFP */
void myTask(void){
	if(button1Status != HAL_GPIO_ReadPin(B1_GPIO_Port, B1_Pin)){

		button1Status = HAL_GPIO_ReadPin(B1_GPIO_Port, B1_Pin);
		NotifyCharData[0] = button1Status;
		Custom_Char2_Send_Notification();
	}
	UTIL_SEQ_SetTask(1<<CFG_TASK_MY_TASK, CFG_SCH_PRIO_0);
}
/* USER CODE END PFP */

3) Modify the fuction:
/* Functions Definition ------------------------------------------------------*/
void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification)
{
 /* USER CODE BEGIN CUSTOM_STM_App_Notification_1 */

 /* USER CODE END CUSTOM_STM_App_Notification_1 */
 switch (pNotification->Custom_Evt_Opcode)
 {
 /* USER CODE BEGIN CUSTOM_STM_App_Notification_Custom_Evt_Opcode */

 /* USER CODE END CUSTOM_STM_App_Notification_Custom_Evt_Opcode */

 /* Service_1 */
 case CUSTOM_STM_CHAR1_WRITE_EVT:
 /* USER CODE BEGIN CUSTOM_STM_CHAR1_WRITE_EVT */

 /* USER CODE END CUSTOM_STM_CHAR1_WRITE_EVT */
 break;

 case CUSTOM_STM_CHAR2_NOTIFY_ENABLED_EVT:
 /* USER CODE BEGIN CUSTOM_STM_CHAR2_NOTIFY_ENABLED_EVT */
 	notifyStatus = 1;
 /* USER CODE END CUSTOM_STM_CHAR2_NOTIFY_ENABLED_EVT */
 break;

 case CUSTOM_STM_CHAR2_NOTIFY_DISABLED_EVT:
 /* USER CODE BEGIN CUSTOM_STM_CHAR2_NOTIFY_DISABLED_EVT */
 	notifyStatus = 0;
 /* USER CODE END CUSTOM_STM_CHAR2_NOTIFY_DISABLED_EVT */
 break;

 case CUSTOM_STM_NOTIFICATION_COMPLETE_EVT:
 /* USER CODE BEGIN CUSTOM_STM_NOTIFICATION_COMPLETE_EVT */

 /* USER CODE END CUSTOM_STM_NOTIFICATION_COMPLETE_EVT */
 break;

 default:
 /* USER CODE BEGIN CUSTOM_STM_App_Notification_default */

 /* USER CODE END CUSTOM_STM_App_Notification_default */
 break;
 }
 /* USER CODE BEGIN CUSTOM_STM_App_Notification_2 */

 /* USER CODE END CUSTOM_STM_App_Notification_2 */
 return;
}

4)Modify the fuction:
void Custom_Char2_Send_Notification(void) /* Property Notification */
{
 uint8_t updateflag = 0;

 /* USER CODE BEGIN Char2_NS_1*/
 updateflag = notifyStatus;
 /* USER CODE END Char2_NS_1*/

 if (updateflag != 0)
 {
 Custom_STM_App_Update_Char(CUSTOM_STM_CHAR2, (uint8_t *)NotifyCharData);
 }

 /* USER CODE BEGIN Char2_NS_Last*/

 /* USER CODE END Char2_NS_Last*/

 return;
}