Skip to main content
DS.4
Senior
Jul 6, 2021 12:54 PM UTC
Solved

STM32WB IPCC

Hi all

Maybe you can help me understand something about the IPCC.

From my understanding: In case CPU2(BlackBox) sends the CPU1 an command:

CPU2(BLE) -----RX occupied ISR -----> CPU1(APP), look in Queue to get the user event.

: CPU1(APP) --------TX free ISR---------> CPU2(BLE) , where is the data??

When CPU1 (APP) gets a user event from CPU2, It sends a response to CPU2 in a form of TX free ISR is sent. Where is the data of that event?

Thanks.

P.s. I see that in the opposite direction the data is stored in pCmdBuffer

This topic has been closed for replies.
Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Jul 19, 2021 10:05 AM UTC

There is no BLE trace sent over IPCC. Only Thread protocol stack (and possibly Zigbee protocol) is sending traces IPCC to the M4 core.

3 replies

Remi QUINTIN
ST Technical Moderator
Jul 16, 2021 4:01 PM UTC

The wireless stack on CPU2 never sends a command to CPU1.

It is the other way. The application running on CPU1 sends a command to CPU2 via IPCC and CPU2 returns data received from the network or answers to previous commands from the application.

Buffers used for inter-processor communication are located in SRAM2.

Attached is a basic description of IPCC.

DS.4
DS.4Author
Senior
Jul 18, 2021 6:55 AM UTC

Thanks,

I see that in code there are 2 ISRs for messages. Both the Async user evet and the RespCmd evnt? What is the difference?

Regarding traces, it is not possible to use the Traces Channel?

I am wondering if there is extra value in creating the channel.

Thanks.

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Jul 19, 2021 10:05 AM UTC

There is no BLE trace sent over IPCC. Only Thread protocol stack (and possibly Zigbee protocol) is sending traces IPCC to the M4 core.