STM32WB FREERTOS FUOTA not working
Hi,
I try to set FUOTA with FREERTOS on NUCLEO-WB55 demo board.
I start with the BLE_HeartRateFreeRTOS, I built it, flash it and all is ok.
Then I flash OTA bootloader (I know it's working also cause I try to update with BLE_p2pServer_ota project and it's ok too)
Finally in BLE_CFG_OTA_REBOOT_CHAR project, I change stm32wb55xx_flash_cm4.ld file with the one with OTA section and I modified ble_conf.h to enable BLE_CFG_OTA_REBOOT_CHAR. But after having being flashed on the STM32WB, nothing work anymore. I check memory and bin have been correcly written at the right address 80007000.
Could somebody help me with this please?