Skip to main content
LSpad.1
Associate III
Jan 27, 2021 12:44 PM UTC
Solved

STM32WB BLE Connection examples v1.10.0

Hi,

i have an STM32WB used as client. Compiling the project with libraries 1.8.0 i can connect 5 BLE servers without any problem, compiling the project with libraries 1.10.0 i can't connect more than 2 BLE Servers, from the third aci_gap_create_connection return 0x41.

I thought that the problem was the STACK Ble not updated, but updating it the problem is still these. Which can be the cause?

Thank you in advance

This topic has been closed for replies.
LSpad.1
LSpad.1Best answer
Associate III
Feb 5, 2021 7:37 AM UTC

The new libraries modify the max link number to 2, so you have to manually change it back to 8.

1 reply

LSpad.1
LSpad.1AuthorBest answer
Associate III
Feb 5, 2021 7:37 AM UTC

The new libraries modify the max link number to 2, so you have to manually change it back to 8.