Skip to main content
SikandarLF
Associate II
Feb 14, 2024 9:16 AM UTC
Solved

STM32WB BLE and EEPROM casuing HardFault

Hi Community

Hope you guys are well. I am trying to implement Bluetooth and emulated eeprom working. i have followed the ble_heartrate_eeprom_emul example and i got blue tooth and eeprom emulation working, the problem i am having is when the EEPROM emulation is implement   my function in custom_stm.c does not work properly, for example when i used any of the GPIO, the controller goes into hard fault, and current went from 0.013A to 0.150A , but as soon as i remove the eeprom emulation code , everything works perfectly. so basically i cant get my things working when there is eeprom emulation , i have tried to release the semaphore 7 in my function but still the same. 

 

there is one more thing, in app_entry.c we have default code , check file attached, 

but the ble heart rate eeprom emulation tell us to put this code, check file attached,

and if i put that code and generate the code again from cubemx it is removed.

Assistance is appreciated!

This topic has been closed for replies.
SikandarLF
SikandarLFBest answer
Associate II
Apr 22, 2024 7:21 AM UTC

i created a support ticket for it. and they coudnt fix it either. so now i am using external eeprom to store data. but thanks for help

 

3 replies

STTwo-32
ST Technical Moderator
Apr 16, 2024 8:13 AM UTC

Hello @SikandarLF 

I've personally tested on the P-Nucleo-WB55 and everything works fine. I suggest you test it using the last Version of the X-Cube and the STM32CubeIDE. If you still have any issue, Please add more details (screenshots, detailed description,...).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SikandarLF
Associate II
Apr 22, 2024 7:19 AM UTC

i have been using the latest version but when the emulated eeprom is implemented, if i try to use any gpio mcu goes into hardfault. but emulated eeprom and ble works fine