Skip to main content
MSpot.1
Associate II
Jul 21, 2020 10:42 PM UTC
Solved

STM32WB and st7789 via spi

I have been trying to get the stm32wb nucleo working with the st7789 lcd but have only observed strange behavior. I have successfully gotten it to work with the stm32f103c8t6 using the code found here. When CPOL=0 on the stm32f103 the screen does not work but on the stm32wb when CPOL=0 the screen will initiate and commands can be sent to it successfully. However when I try to send a frame nothing happens. I have also checked that the DC pin is working as it should. I am confused by the strange behavior observed when CPOL=0, other than that, this is the only thing I have observed when using the stm32wb.

This is the only code changed between the two projects:

Original GPIOInit code (stm32f103):

void st7789_GPIOInit(void) {
	// Enable GPIOA and SPI1 clock
	RCC->APB2ENR |= RCC_APB2ENR_IOPAEN | RCC_APB2ENR_SPI1EN;
	// Enable DMA1 channel
	//RCC->AHBENR |= RCC_AHBENR_DMA1EN;
 
	// Enable SPI
	ST7789_SPI->SR = 0;
	// Reverse polarity?
	ST7789_SPI->CR1 = \
		SPI_CR1_SSM | \
		SPI_CR1_SSI | \
		SPI_CR1_MSTR | \
		SPI_CR1_CPOL | \
		SPI_CR1_BIDIMODE | \
		SPI_CR1_BIDIOE;
	ST7789_SPI->CR1 |= SPI_CR1_SPE;
	
	// DC and RST signals
	// Maximum output speed
	ST7789_DC_PORT->CRH |= GPIO_CRH_MODE8;
	ST7789_RST_PORT->CRH |= GPIO_CRH_MODE9;
	// Output push pull
	ST7789_DC_PORT->CRH &= ~(GPIO_CRH_CNF8);
	ST7789_RST_PORT->CRH &= ~(GPIO_CRH_CNF9);
 
	// SPI pins
	// Maximum output speed on PA5/PA7
	GPIOA->CRL |= GPIO_CRL_MODE5;
	GPIOA->CRL |= GPIO_CRL_MODE7;
	// Alternate mode on PA5/PA7
	GPIOA->CRL = (GPIOA->CRL & ~(GPIO_CRL_CNF5)) | (GPIO_CRL_CNF5_1);
	GPIOA->CRL = (GPIOA->CRL & ~(GPIO_CRL_CNF7)) | (GPIO_CRL_CNF7_1);
}

Ported code (stm32wb):

void st7789_GPIOInit(void) {
	//setup the clocks
	RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;
	RCC->APB2ENR |= RCC_APB2ENR_SPI1EN;
 
	//configure PA1 and PA7 as alternate function
	GPIOA->MODER &= ~(GPIO_MODER_MODE1 | GPIO_MODER_MODE7);
	GPIOA->MODER |= (GPIO_MODER_MODE1_1 | GPIO_MODER_MODE7_1);
 
	//configure PA1 and PA7 to spi mode
	GPIOA->AFR[0] &= ~(GPIO_AFRL_AFSEL1) | (GPIO_AFRL_AFSEL7);
	GPIOA->AFR[0] |= (5U << GPIO_AFRL_AFSEL1_Pos) | (5U << GPIO_AFRL_AFSEL7_Pos);
 
	//configure data/command pin as output
	ST7789_DC_PORT->MODER &= ~(GPIO_MODER_MODE8);
	ST7789_DC_PORT->MODER |= GPIO_MODER_MODE8_0;
	//configure reset pin as output
	ST7789_RST_PORT->MODER &= ~(GPIO_MODER_MODE9);
	ST7789_RST_PORT->MODER |= GPIO_MODER_MODE9_0;
 
	//configure spi
	SPI1->CR1 |= SPI_CR1_SSM | SPI_CR1_SSI | SPI_CR1_MSTR | SPI_CR1_BIDIMODE | SPI_CR1_BIDIOE;
	//SPI1->CR1 |= SPI_CR1_CPOL;
 
	SPI1->CR1 |= SPI_CR1_SPE;
 
}

Other cool code stuff:

void st7789_StartCommand(void) {
	st7789_WaitNanosecs(10); // D/CX setup time
	ST7789_DC_PORT->ODR &= ~ST7789_DC_PIN;
}
void st7789_StartData(void) {
	st7789_WaitNanosecs(10); // D/CX setup time
	ST7789_DC_PORT->ODR |= ST7789_DC_PIN;
}
void st7789_WriteSpi(uint8_t data) {
	for (int32_t i = 0; i<10000; i++) {
		if (ST7789_SPI->SR & SPI_SR_TXE) break;
	}
	ST7789_SPI->DR = data;
	while (ST7789_SPI->SR & SPI_SR_BSY);
}

Both MCUs are clocked at 64 MHz and I have tried different SPI baud rates with no success. Both projects do not use DMA for more simplicity while debugging.

Please tell me if there is any more information I need to provide.

Thank you.

This topic has been closed for replies.
MSpot.1
MSpot.1Best answer
Associate II
Jul 24, 2020 1:37 AM UTC

The problem was it was sending 16 clock cycles instead of 8:

The ST7789_SPI->DR = data

should have been changed to:

*(__IO uint8_t *)&SPI1->DR = data

https://community.st.com/s/question/0D50X00009Xkfrt/spi-8bit-data-length

1 reply

MSpot.1
MSpot.1AuthorBest answer
Associate II
Jul 24, 2020 1:37 AM UTC

The problem was it was sending 16 clock cycles instead of 8:

The ST7789_SPI->DR = data

should have been changed to:

*(__IO uint8_t *)&SPI1->DR = data

https://community.st.com/s/question/0D50X00009Xkfrt/spi-8bit-data-length