Associate II
Apr 4, 2024 12:52 AM UTC
Solved
STM32WB about BLE
- 1 reply
- 811 views
Hello,
I made 2 project about client and server using stm32wb1mmc product.
> server project is using "custom p2p server"
It works well but I want to improve usability.
1. How to reduce scan time for connect client to server?
> I quote it from examples. use "CFG_TASK_START_SCAN_ID" when external pin interrupt is set.
so when button is pushed, client start scan request. after 10s appx, client can be connected server.
I want to reduce this time.
2. How to enter sleep(stop) mode cpu2?
As far as I know, cpu2 can't enter stop mode after cpu1 & cpu2 booted completely. If it is correct, is it no way to cpu2 enter sleep and wake up?
I attached 2 project files.
best regard.