Skip to main content
maciej_zawodniok
Associate
Nov 24, 2014 7:10 PM UTC
Question

stm32w108cb - issue with TX in SimpleMac v2.0.1

Posted on November 24, 2014 at 20:10

Hi,

I'm using Dizic radio modules (STM32W108CB based ones) with SimpleMac v2.0.1 library.

Overall, the example projects work with exception of packet transmission (802.15.4). Every time it accepts the packet transmission with ST_RadioTransmit() but always ends with ''NO ACK'' case in callback function. Also, nothing is received in other modules (even in promiscuous mode).

I've tested it with XBee module and the STM32W/simplemac receives the packets from the XBee. But never transmits anything. No error but NO ACK is given.

#stm32w-wireless-simplemac
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    Nov 24, 2014 7:33 PM UTC
    Posted on November 24, 2014 at 20:33

    There's really no support here for the STM32W108 devices.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..