Skip to main content
Darren Hogan
Visitor II
May 28, 2018 8:41 PM UTC
Question

STM32L476RG + IDW01M1 - WiFi hangs before connecting

Posted on May 28, 2018 at 22:41

Hi! I'm looking for some help in getting my STM32L476RG and IDW01M1 up and running with the FP-CLD-AZURE1 STM32Cube function pack. I also have the sensors.

I've flashed the board with the relevant binaries etc... The Azure_Sns_DM program accepts my azure and WiFi variables but just seems to hang after getting to the connection string:

Output below:

UART Initialized

I2C Initialized

STMicroelectronics Azure_Sns_DM:

Version 3.3.0

STM32L476RG-Nucleo board

Azure SDK Version 1.1.31

Ok Accelero Sensor

Ok Gyroscope Sensor

Ok Magneto Sensor

Ok Humidity Sensor

Ok Temperature Sensor1

Ok Temperature Sensor2

Ok Pressure Sensor

Enabled Accelero Sensor

Enabled Gyroscope Sensor

Enabled Magneto Sensor

Enabled Humidity Sensor

Enabled Temperature Sensor1

Enabled Temperature Sensor2

Enabled Pressure Sensor

(HAL 1.8.2_0)

Compiled May 26 2018 08:21:23 (openstm32)

OTA with one HTTP HEAD + Multiple HTTP one GET of 1024Bytes

Testing BootLoaderCompliance:

Version 1.2.0

BL Version Ok

MagicNum Ok

MaxSize 0x7c000

OTAStartAdd Ok

BootLoader Compliant with FOTA procedure

Init Application's Timers

Init Random Number Generator

Enabled Free Fall

Init WIFI's Timers

Init WIFI's UART1

--------------------------

| WIFI Credential |

--------------------------

Meta Data Manager read from Flash

Meta Data Manager version=0.8.0

Generic Meta Data found:

WIFI Size=81 [bytes]

AZURE Size=256 [bytes]

Default SSID : <redacted>

Default PassWd : <redacted>

Default EncMode: WPA2/WPA2-Personal

Wait 3 seconds for allowing User Button Control for changing it

--------------------------

| Connection String |

--------------------------

Default Connection String : <redacted>

Wait 3 seconds for allowing User Button Control for changing it

I can't for the life of me see whats going on after this point - AT commands don't seem to work.

If I could get some debug from the terminal that might give me a clue - but as I'm a newbie at all this I'm struggling...

Any help appreciated!

Thanks

Darren

#stm32-wifi #idw01m1
    This topic has been closed for replies.