Skip to main content
This topic has been closed for replies.
Philippe Cherbonnel
ST Employee
July 19, 2022

Hello,

A regression has been introduced in release v1.2.0.

Issue:

In case of high frequency ratio between CPU and ADC (CPU high frequency, ADC low frequency), function HAL_ADCEx_Calibration_Start() returns an error.

Root cause:

A delay must be fullfilled between ADC enable and ADC disable.

Fix:

In function HAL_ADCEx_Calibration_Start(), a delay must be added:

  LL_ADC_Enable(hadc->Instance);

<delay here>

  LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);

  LL_ADC_Disable(hadc->Instance);

The fix will be available in next STM32WL FW package release.

Documentation is being updated to mention this constraint.

Best regards

Philippe

12 replies

John1960
John1960Author
Associate
May 31, 2022

Sorry, MCU STM32WLE5

Louis AUDOLY
ST Employee
June 6, 2022

Hello and welcome @John1960​ ,

You can have a look at the example ADC_AnalogWatchdog that you can find here :

STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Examples\ADC\ADC_AnalogWatchdog

In the main function there is a calibration that don't return an error.

Which code are you running ?

Best regards

John1960
John1960Author
Associate
June 6, 2022

I use my own code, which use ADC. First I want to calibrate it, so I call HAL_ADCEx_Calibration_Start. 

I began from stm32cubewl_v1-1-0, and it worked well.

Then I upgaded library to stm32cubewl_v1-2-0, and the function began to return HAL_ERROR.

Functions HAL_ADCEx_Calibration_Start  from version 1.1 and from version 1.2 are extreemly different.

Part of my code - Green LED is ON:

void ADC_Init ()

{

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;

 PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_HSI;

 if ( HAL_RCCEx_PeriphCLKConfig ( &PeriphClkInitStruct ) != HAL_OK )

  {

   Error_Handler();

  }

 /* Peripheral clock enable */

 __HAL_RCC_ADC_CLK_ENABLE();

 hadc.Instance = ADC;

 hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV64;

 hadc.Init.Resolution = ADC_RESOLUTION_12B;

 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;

 hadc.Init.ScanConvMode = ADC_SCAN_DISABLE;

 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

 hadc.Init.LowPowerAutoWait = DISABLE;

 hadc.Init.LowPowerAutoPowerOff = DISABLE;

 hadc.Init.ContinuousConvMode = DISABLE;

 hadc.Init.NbrOfConversion = 1;

 hadc.Init.DiscontinuousConvMode = DISABLE;

 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;

 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

 hadc.Init.DMAContinuousRequests = DISABLE;

 hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;

 hadc.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;

 hadc.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;

 hadc.Init.OversamplingMode = DISABLE;

 hadc.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;

 if (HAL_ADC_Init(&hadc) != HAL_OK)

 {

  Error_Handler();

 }

 /* ADC interrupt Init */

 HAL_NVIC_SetPriority(ADC_IRQn, 0, 0);

 HAL_NVIC_EnableIRQ(ADC_IRQn);

// return;

 if (HAL_ADCEx_Calibration_Start(&hadc) != HAL_OK)

 {

  /* Calibration Error */

 GreenLED_On ();

  Error_Handler();

 }

 } // ADC_Init

Philippe Cherbonnel
ST Employee
July 19, 2022

Hello,

A regression has been introduced in release v1.2.0.

Issue:

In case of high frequency ratio between CPU and ADC (CPU high frequency, ADC low frequency), function HAL_ADCEx_Calibration_Start() returns an error.

Root cause:

A delay must be fullfilled between ADC enable and ADC disable.

Fix:

In function HAL_ADCEx_Calibration_Start(), a delay must be added:

  LL_ADC_Enable(hadc->Instance);

<delay here>

  LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);

  LL_ADC_Disable(hadc->Instance);

The fix will be available in next STM32WL FW package release.

Documentation is being updated to mention this constraint.

Best regards

Philippe

Dana Myers
Senior
September 10, 2022
 /* Apply calibration factor */
 LL_ADC_Enable(hadc->Instance);
 
 while (!LL_ADC_IsActiveFlag_ADRDY(hadc->Instance))
 	/* spin */;
 LL_ADC_ClearFlag_ADRDY(hadc->Instance);
 
 LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
 LL_ADC_Disable(hadc->Instance);

As above, I spin on ADRDY, no need for a timer

Motla1
Associate II
September 11, 2022

I reported the issue for STM32CubeWB as well.

The library already have some macros that wait for ADRDY the flag, just remove the LL_ prefix:

 /* Apply calibration factor */
 ADC_Enable(hadc);
 LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
 ADC_Disable(hadc);

https://github.com/STMicroelectronics/STM32CubeWB/issues/59

John1960
John1960Author
Associate
July 19, 2022

OK

MechMan
Explorer
April 13, 2023

Hi. I have this problem with stm32g07, but only -Og compile flag. The solution the same, Delay after Enable or use ADC_Enable

Dana Myers
Senior
April 13, 2023

is there a plan / what is the plan to roll out a fix for this? Using FW 1.3 I still see this.

Thanks -

Dana