STM32CubeProgrammer 2.9.0 + USART + STM32WLE5, appears to truncate binary on a 4k boundary
I am programming an STM32WLE5CCU6 using STM32CubeProgrammer v2.9.0 and USART / embedded bootloader. Without exception, every binary I attempt to program (ELF or bin does not matter) is truncated at a 4k boundary (0x1E000 in one case, 0x14000 in another). The last portion of the binary is not programmed to the MCU.
Using the ST-Link v2 on the same part, programming is successful. Binaries are produced with STM32CubeIDE v1.8.0 using the built-in ARM GCC toolset.
This very much looks like a bug in STM32CubeProgrammer v2.9.0