Skip to main content
Associate
Oct 27, 2023 10:17 AM UTC
Solved

STM32CubeMonitor-RF for testing BLUENRG-M2SP

Hi,

I want to use the BLUENRG-M2SP for an application and I want to test this BLE module before designing a HW. For this, I have a NUCLEO F411RE and a NUCLEO BNRG2A1.

I wonder if it's possible to use STM32CubeMonitor-RF as a serial terminal in order to send ACI commands from a computer to the BNRG2A1 thorugh the USB dongle provided with the P-NUCLEO-WB55.

Thanks in advanced,

David

This topic has been closed for replies.
Laurent LOUAZON
Laurent LOUAZONBest answer
ST Employee
Nov 13, 2023 3:34 PM UTC

Hello,

 

No, cubeMonitorRF tool cannot be used.

You should use the BlueNRG GUI PC tool (STSW-BNRGUI - BLUENRG family GUI - STMicroelectronics) that will do the same.
It is normally intended to be used with Nucleo-L476RG flashed with Virtual COM port available in X-CUBE-BLE2 package.

You then should port this application for your NUCLEO F411RE, then you 'll be able to use the GUI for sending ACI command from the PC.

 

Regards
Laurent

 

1 reply

Laurent LOUAZON
Laurent LOUAZONBest answer
ST Employee
Nov 13, 2023 3:34 PM UTC

Hello,

 

No, cubeMonitorRF tool cannot be used.

You should use the BlueNRG GUI PC tool (STSW-BNRGUI - BLUENRG family GUI - STMicroelectronics) that will do the same.
It is normally intended to be used with Nucleo-L476RG flashed with Virtual COM port available in X-CUBE-BLE2 package.

You then should port this application for your NUCLEO F411RE, then you 'll be able to use the GUI for sending ACI command from the PC.

 

Regards
Laurent