Skip to main content
DS.4
Senior
Nov 14, 2021 8:54 PM UTC
Solved

STM32CubeMonitor-RF DLL or CLI

Hi everyone,

I am trying to create a windows pc app to talk to the STM32WB board using the dongle.

I want to run some scripts, e.g., write to characteristic, connect, read an etc.

I saw that STM32CubeMonitor-RF can already run scripts via some text files. I wonder if it is possible to run the script text file from the CLI, or better talk to the dongle via some sort of .dll interface.  The second would the preferable way .

Thanks

This topic has been closed for replies.
Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Mar 31, 2022 11:16 AM UTC

Hello @Community member​ 

STM32CubeMonitorRF can run only text script in a proprietary syntax. It cannot be used through CLI

We are currently studying the feasibility of running script from CLI or through other external way like Python.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Mar 31, 2022 11:16 AM UTC

Hello @Community member​ 

STM32CubeMonitorRF can run only text script in a proprietary syntax. It cannot be used through CLI

We are currently studying the feasibility of running script from CLI or through other external way like Python.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.