Skip to main content
Associate
Dec 10, 2025 6:26 AM UTC
Question

STM32CubeIDE v 1.19.0 log redirection on uart in BLE application of STM32WB05KZ Problem

I am working on custom evk of STM32WB05KZ sdk(stm32cubewb0-v1-3-0) on STM32CubeIDE_v_1.19.0 and STM32CubeProgrammer and trying to redirect logs on UART1 through __io_putchar/_write. It is working with Examples(GPIO_EXT, I2C, ADC, etc) but while running BLE(Any of it) section from Applications it is not giving any log through UART/Virtual COM Port. Below is the refrenced code of my main.c:

 
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/

#include "main.h"
#include "pka.h"
#include "radio.h"
#include "radio_timer.h"
#include "usart.h"
#include "gpio.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
//#include "stm32wb0x_ll_pwr.h"

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

void PeriphCommonClock_Config(void);

/* USER CODE BEGIN PFP */

#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

int __io_putchar(int ch)
{
HAL_UART_Transmit(&huart1, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
return ch;
}
//int _write(int file, char *ptr, int len)
//{
// HAL_UART_Transmit(&huart1, (uint8_t*)ptr, len, HAL_MAX_DELAY);
// return len;
//}
/* USER CODE END 0 */
/**

* @brief The application entry point.
* @retval int
*/

int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */

/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

/* USER CODE BEGIN Init */

/* USER CODE END Init */

/* Configure the system clock */

SystemClock_Config();

/* Configure the peripherals common clocks */

PeriphCommonClock_Config();

/* USER CODE BEGIN SysInit */

/* USER CODE END SysInit */

/* Initialize all configured peripherals */

MX_GPIO_Init();
MX_RADIO_Init();
MX_RADIO_TIMER_Init();
MX_PKA_Init();
MX_USART1_UART_Init();

/* USER CODE BEGIN 2 */

// Disable BLE low-power that breaks UART

// int a=10;
// int b=20;
// printf("Sum: %d\n", a+b);
// printf("BLE Init Started\r\n");

/* USER CODE END 2 */

/* Init code for STM32_BLE */

MX_APPE_Init(NULL);

/* Infinite loop */

/* USER CODE BEGIN WHILE */

// Prevent BLE stack from putting MCU in DEEPSTOP
// LL_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN + 1); // Force exit from deepstop
// LL_PWR_EnablePUPDCfg(); // Maintain IO levels
// printf("Low power disabled\r\n");

while (1)
{
/* USER CODE END WHILE */

MX_APPE_Process();

/* USER CODE BEGIN 3 */

printf("ble init done!..\r\n");
uint8_t msg[] = "Raw UART\r\n";
HAL_UART_Transmit(&huart1, msg, sizeof(msg)-1, 100);
HAL_Delay(500);

//
// printf("Hello Atul\n");
// HAL_Delay(2000);

}

/* USER CODE END 3 */
}

/**

* @brief System Clock Configuration
* @retval None

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

/** Configure the SYSCLKSource and SYSCLKDivider

*/

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_RC64MPLL;
RCC_ClkInitStruct.SYSCLKDivider = RCC_RC64MPLL_DIV2;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_WAIT_STATES_0) != HAL_OK)
{
Error_Handler();
}

}

/**

* @brief Peripherals Common Clock Configuration
* @retval None

*/

void PeriphCommonClock_Config(void)

{

RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

/** Initializes the peripherals clock

*/

PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS;
PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLK_DIV4;

if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)

{
Error_Handler();
}

}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**

* @brief This function is executed in case of error occurrence.
* @retval None

*/

void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();

while (1)

{
}

/* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None

*/

void assert_failed(uint8_t *file, uint32_t line)
{

/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

Error_Handler();

/* USER CODE END 6 */

}
#endif /* USE_FULL_ASSERT */