Skip to main content
Visitor II
Mar 18, 2026 5:41 AM UTC
Question

Stm32 WLE JC WioE5 SUBGHZ PHY HAL Delay , HAL_GetTick() does no work..

Hello. We are developing a p2p application using two Wio-E5 mini modules based on stm32 WLE5JC.
The problem I'm facing is HAL_DELAY not working.

I created the project, chose HSE, LSE, then SysTick, and then after I selected SysTick, HAL_IncTick() was well declared in SysTick_Handler, and I also checked NVIC. But when I do HAL_GetTick() at any moment, I get zero. Isn't there a problem with this??
The Ping Pong example also uses HAL_Delay, but I cannot understand why this happened. 

This is very critical for my project becaude when i set modem state in RX, it call timeout in next loop. please help me

1 reply

ST Technical Moderator
Apr 9, 2026 11:56 AM UTC

Hello @David16255 ,

Try enabling global IRQs and check the SysTick interrupt priority that have a higher priority than any peripheral interrupt. Also, make sure the interrupt handler is not blocked or masked.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks