Skip to main content
Karthi
Associate II
May 28, 2023 8:13 AM UTC
Question

STLINK-V3PWR

 STLINK-V3PWR Not able to connect to STM32WL and other STM32 MCU's using STM32CubeProgrammer

Same MCU is working with STlink-V3

 13:39:13 : ST-LINK SN : 002F004D3431510137383732

 13:39:13 : ST-LINK FW : V4J2B1P4

 13:39:13 : Board    : STLINK-V3PWR

 13:39:13 : Voltage   : 0.02V

 13:39:13 : Error: No STM32 target found

This topic has been closed for replies.

2 replies

S.Ma
Principal
May 28, 2023 6:35 PM UTC

Apparently the measured Target MCU voltage is 0.02V, maybe there are some jumpers of switch to adjust to get setup working well.

Karthi
KarthiAuthor
Associate II
May 29, 2023 11:13 AM UTC

Hi

I able to connect now using CubeProgrammer, After connecting TVCC to Target MCU VCC.

Without connecting TVCC to MCU VCC , STlink-V3 is working but not with V3PWR.

again V3PWR is still not working with CubeMX IDE.

Thanks

KarthiG